Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Connect to eMoticom eM007 ECU

I have an eMoticom eM007 ECU on a motorcycle which has been developed from the SPC5-L9177A-K02 dev kit. I wish to connect to the ECU to download the bin file so I can learn to tune it. The ECU has a canbus connector with 4 pins +12v, Gnd, CAN-H, and ...

Ian Lowe by Associate II
  • 6124 Views
  • 9 replies
  • 5 kudos

How to send can messages with different cycles in spc5 studio?

hello~ I am using the spc58ec disp chip and want to continuously send CAN messages of different cycles. Here is the code what i wrote: //// void send_10ms(){     uint32_t rv;     CANTxFrame msg_10ms;     msh_10ms.ID = 0x11U;     msh_10ms.DLC = 8U;   ...

Resolved! Set Life Cycle

I am using the SPC58 MCU product with the TRACE32 debugger. When changing the Life Cycle from "customer_delivery" to "in_field" with the trace32 script, debugging is only possible by entering the keycode. What should I do if I want to change the Life...

hgh by Associate
  • 2147 Views
  • 2 replies
  • 1 kudos

Resolved! SPC58EC with Flash driver

Hello, I am currently struggline with flash program with some tools.The tool send 62byte data with CAN FD and I want to write down it.I am using SPC5Studio with Flash_driver (ssd_c55.h)* FILE NAME : ssd_c55.h ** DATE : December 19, 2011 ** AUTHOR : F...

otcagon by Associate II
  • 3041 Views
  • 3 replies
  • 0 kudos

Programming guide for Stellar

Hi, Good day. This is third party for programmer.Our customer requires the programming for SR5E1-176, and we need the programming guide to develop the programming board and algorithm. Could you help to share the programming guide to me?or Please let ...

JHsu.14 by Associate II
  • 1111 Views
  • 0 replies
  • 0 kudos

Resolved! StellarStudio targetting SR6G7

Hello,I want to build a simple application (like a UART message, GPIO bit-bang etc.) targeting SR6G7 and running on a custom board. To support that I want to use the latest SDK 3.3.0 and flash the code via StellarLINK.Is there any guide how to add th...

savo by Associate
  • 2157 Views
  • 1 replies
  • 0 kudos

Resolved! Set Life Cycle

I am using the SPC58 MCU product with the TRACE32 debugger. When changing the Life Cycle from "customer_delivery" to "in_field" with the trace32 script, debugging is only possible by entering the keycode. What should I do if I want to change the Life...

hgh by Associate
  • 1711 Views
  • 1 replies
  • 0 kudos