Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC560P chip id

The chip I am using is SPC560P, please how can I do it to get the chip ID?

wybll by Associate
  • 1430 Views
  • 1 replies
  • 0 kudos

SPC574K

I am working on the development of SPC574K chip, but the debugger cannot connect with the chip successfully. When the chip is powered on, the crystal waveform is the first picture, which is normal. When I press the reset button or the connect button...

微信图片_20240603164008.jpg 微信图片_20240603163958.jpg
Shiyu by Associate
  • 1630 Views
  • 1 replies
  • 0 kudos

Resolved! Embedded virtualization with SR6X7

Hi, I am trying out embedded virtualization with SR6X7, i have SR6X7 ZCU demo board with me. I am very new this this dev environment. could someone help me with embedded virtualization related docs.    Thanks in advance. Prabhu

Resolved! SPC58 performance

Hello,I created a new project using default settings only to toggle an OUTPUT just to see the microcontroller performance.I monitored that outpup with an oscilloscope and I get only 4.17MHz.I am using a SPC58NH-DISP.Is that an expected output frequen...

Resolved! BSDL file for Stellar Integration MCU

Hello, I want to do a boundary-scan test for a SIP module which uses ST Stellar Integration MCU SR6Gx series, how can I get its BSDL file?

fengyun by Associate
  • 1624 Views
  • 1 replies
  • 0 kudos

Resolved! I want to debug my SPC563M64 board in SPC5studio. What should I do?

I want to debug my SPC563M64 board in SPC5studio. What should I do? I will go there to obtain support files for boards like SPC58NG 1>C:\SPC5Studio-6.0\openocd\scripts\board\spc58NG_dis.cfg2>C:\SPC5Studio-6.0\openocd\scripts\target\spc58ng.cfg3>C:\SP...

xqing.1 by Associate II
  • 3829 Views
  • 6 replies
  • 0 kudos

Resolved! Flashing directly into MCU

Hello Experts,I have AEK-MCU-SPC5LNK debugger and want to flash .hex/.out file directly into controller SPC582B.how can I do this. please share necessary step guide. I don't want to use any IDE like using debug mode to dump the code.   Waiting for re...

Resolved! DSPI parameter configuration issue of SPC5

Hello! I would like to ask what each of the three modes in the picture below represents?Also, what does it mean if the GPIO parameter is set to PORT_1? I did not see that the GPIO bit 0 for this PORT_1 port is in use in the pin configuration editor! ...

QQ图片20240515103352.png
Bwang.3 by Associate III
  • 1649 Views
  • 1 replies
  • 0 kudos