Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! changing dcf records

hi i am new to the controller, i read the manual that dcf records contains the configurations like if device boots up it performs some basic tests and then basis on the application address provided in dcf record, it jumps to application, but that add...

saka645 by Associate
  • 2111 Views
  • 2 replies
  • 0 kudos

How to debug FreeRTOS network status in SPC5Studio?

Dears,When debugging SPC58N's network function. When I add printf function using RUN IO components.It always crash. I want to ask how to debug freeRTOS TCPIP protocol? which method to check how to get statistics info and etc.Thanks for help.

frankbi by Associate II
  • 1789 Views
  • 2 replies
  • 0 kudos

SPC5 STDIO build error

Hello, As shown in figure, I import a samples project, compile failure hint "make: * * * [components/spc560pxx_platform_component_rla/lib/RSC/rules. Mk: 164: elf] Error 1 "How do I solve it,T  

wybll_0-1718353217761.png
wybll by Associate
  • 1281 Views
  • 1 replies
  • 0 kudos

Resolved! I want to test the SPC5-FLASHER program.

I want to test the SPC5-FLASHER program.When installing the program, you must register the serial number.How can I get a serial number assigned?Should I send the saved information by e-mail after recording the serial number request information during...

Mingus by Associate
  • 3007 Views
  • 4 replies
  • 0 kudos

Resolved! SPI frame size more than 4 bytes

HelloI working with spc560p and I send or receive with SPI very good and had no problem, but if I want to send or receive more than 4 bytes (32bits) in one message (one chip select), what should I do? I used this format for send and receive: spi_lld_...

DNewm.1 by Associate III
  • 2682 Views
  • 2 replies
  • 1 kudos

SPC5-UDEBUG

We have bought SPC5-UDEBUG-TL license to be able to debug SPC58EE80 MCU.By description"Supports both SPC5-UDESTK standalone and the equivalent version embedded into Discovery board.Supports SPC5x MCUsSupports Multicore, eTPU and GTM debuggingIncludes...

MBedl.1 by Associate II
  • 1839 Views
  • 2 replies
  • 0 kudos

The SPC58 MCU has no responsing for the PORST reset

The mcu of SPC58 does not response the PORST reset. I knew one case that the mcu actives the reset escalation, but  MC_RGM.FRET.R and MC_RGM.DRET.R  have been set 0; I want know other possiable reason ?This problem confused me long time.  Thank you f...

YYM by Associate
  • 1670 Views
  • 2 replies
  • 0 kudos