2014-06-20 2:41 AM
C90FL program fails due to alignment error but all parameters check out?
Parameter details before call:dest size source result = C90FL_ERROR_ALIGNMENT0x00008000 0x00000100 0x40005300 0x000001000x00008100 0x00000100 0x40005300 0x00000100From UM1627, p.15, table 18, Troubleshooting for FlashProgram()C90FL_ERROR_ALIGNMENTThis error indicates that dest/size/source isn�t properly alignedCheck if dest and size are aligned on double word (64-bit) boundary. Check if source is aligned on word boundary.Ok my checks,0x8000 & 8 = 0 so aligned to 64bit/double word boundary0x100 & 8 = 0 so aligned to 64bit/double word boundary0x40005300 & 8=0 or 0x40005300 & 4=0 source is aligned to 32bit and 64bit brounaryWhat else should be check?Blank check and then erase before hand worked so the flash is ready for programming.Here is the VLE?? code I have been using for program from C90FL library, beta.My development device is spc560b64l7.const unsigned long FlashProgram_C[] = { 0x0080D101, 0x18210690, 0x1A61093C, 0x7C000026, 0xDE01013F , 0x014D015B, 0x026F027E, 0x488A4809, 0xC0EF7FB5, 0xDB78329F , 0x00207E75, 0xA3967E93, 0xA1D67E94, 0xA8501874, 0xA8007A0E , 0x001076F4, 0x07BF1874, 0xA8007A1E, 0x000A6379, 0x7800028E , 0x529F000C, 0x52BF0010, 0x7E94AA14, 0x5681001C, 0x529F0004 , 0x52BF0008, 0x7E94AA14, 0x56810018, 0x7F9DDA14, 0x529F000C , 0x7D9DA040, 0x7A1C0032, 0x5281001C, 0x7D9DA040, 0x7A0C0026 , 0x529F0010, 0x7D9BA040, 0x7A1D001A, 0x5281001C, 0x7D9CA040 , 0x7A1D000E, 0x72600001, 0x36610010, 0xE821529F, 0x00047D9D , 0xA0407A1C, 0x00325281, 0x00187D9D, 0xA0407A0C, 0x0026529F , 0x00087D9B, 0xA0407A1D, 0x001A5281, 0x00187D9C, 0xA0407A1D , 0x000E7260, 0x00023661, 0x0010E804, 0x63697800, 0x01F0187B , 0xA8007A1E, 0x01E8529E, 0x00005681, 0x00205281, 0x00201A94 , 0xC8161874, 0xA8007A1E, 0x000C7320, 0x03007800, 0x01C8529E , 0x00001A94, 0xD0107694, 0x049F569E, 0x0000329F, 0x002018F4 , 0xA8207A0E, 0x000E777C, 0xD97F4A0A, 0x4888E821, 0x329F0020 , 0x18F4A810, 0x7A0E000E, 0x777CE13F, 0x490A4888, 0xE816329F , 0x002018F4, 0xA8087A0E, 0x000E777C, 0xE8FF488A, 0x4888E80B , 0x329F0020, 0x18F4A804, 0x7A0E000C, 0x777CF0BF, 0x484A4848 , 0x72600001, 0x56610024, 0xE86118FA, 0xA8047A0D, 0x001652B7 , 0x00005297, 0x0004569D, 0x000456BD, 0x0000E805, 0x52970000 , 0x569D0000, 0x048D7EF7, 0xC2147E9D, 0xD3967E94, 0xD1D67E94 , 0xE8501874, 0xA8007A1E, 0x00105281, 0x00247D94, 0xE0407A0E , 0x0070529E, 0x00001A94, 0xD0017694, 0x049F569E, 0x0000E80C , 0x727F7FFF, 0x7D969840, 0x7A1E000E, 0x7ECCB378, 0x7D8903A6 , 0x0007529E, 0x00007694, 0x056B1874, 0xA8007A1E, 0xFFDE529E , 0x00007694, 0x05AD1874, 0xA8007A0E, 0x0018527E, 0x00007673 , 0x003D7673, 0x049F567E, 0x00006359, 0xE815529E, 0x00007694 , 0x003D7694, 0x049F569E, 0x00005281, 0x00241E94, 0x00015681 , 0x00245281, 0x00247D94, 0xE0407A0D, 0xFF38527E, 0x00007673 , 0x07357673, 0x049F567E, 0x0000527F, 0x000070F3, 0x940818F3 , 0xA9C07A1E, 0x00307278, 0xE3F95273, 0x801C5661, 0x00147278 , 0xE3F95273, 0x801C7674, 0x003D7278, 0xE3F95693, 0x801C5261 , 0x00147298, 0xE3F95674, 0x801C527F, 0x000070F3, 0x940818F3 , 0xA9C07A0E, 0x00307278, 0xE3F95273, 0x80205661, 0x00147278 , 0xE3F95273, 0x80207674, 0x003D7278, 0xE3F95693, 0x80205261 , 0x00147298, 0xE3F95674, 0x8020527F, 0x00241873, 0xA8007A1E , 0x00060002, 0x01935181, 0x00387D8F, 0xF1201A61, 0x083CC011 , 0xC1010090, 0x00040000 , 0x30393530, 0x34464646 }; /* Total Size = 194 words */ #c90fl2014-06-30 2:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.