Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Bootloader code

Posted on March 20, 2017 at 15:58Hi All,I am new to SPC family micro controllers,I am using SPC560B- Discovery board,I need a boot-loader sample code, which will be reading the binary file data over a UART,It will be very helpful if any one shares s...

Resolved! Error in the test application??? SPC5Studio

Posted on March 21, 2017 at 17:07I'm using the test application 'STM test Application for discovery'  and also if i never used it, when i want to compile it i have this 3 errors:FMPLL-IN has a value (0) out of range: [4000000,64000000] configuration...

Problem in Writing to EED-EEPROM

Posted on March 20, 2017 at 15:47Hello All, I am working on SPC560Bxx Discovery board using SPC5studio version 5.2.1.EED test code for SPC560B- Discovery RLA is working as described in ''readme'' file.As per my understanding FSL_WriteEeprom writes 1...

0690X00000606TnQAI.png

Debugger access locked out?

Posted on March 10, 2017 at 15:52Hi, is it possible to lock out debugger access after programming the DCF record in the UTEST memory region?I am using the SPC570S40E1 micro and the Lauterbach debugger. After programming a DCF record incorrectly, I a...

Resolved! config libreries missing

Posted on March 13, 2017 at 09:58Hi all,I'm new to the enviroment so I'm sorry to be so newbie.Last Friday I was using a test application to get started and at the first attempt i could flash the program and everything was fine. Now I open SPC5Sudio...

Resolved! Clock and PLL initialization

Posted on March 03, 2017 at 21:52 Hi, I amtrying to setup the clocks/PLL on the SPC570S40E1 microcontroller.I would like use the PLL0 as the system clock. Here is my configuration: AC3 SC -> 16Mhz IRSOC AC2 SC -> PLL1 PLL0 Settings:...

0690X00000606RhQAI.png

eSCI uart receive bit order

Posted on March 09, 2017 at 10:44Hi,Refer to reference manual RM0029 Page1362, while using eSCI as UART mode,1) for SCI data register eSCI_DR,what's meaning for two lines below 15:0(R), 0:15(W)?2) while bit sequence D0->D7(10101101) received on UART...

0690X00000606WgQAI.png
270284440 by Associate III
  • 1580 Views
  • 2 replies
  • 0 kudos

SPC5-UDESTK adapter voltage source

Posted on March 02, 2017 at 15:33I have an SPC5-UDESTK JTAG adapter here, which I am using with UDE.Does the adapter source it's own voltage, or do I need to feed voltage from the target back to it? If so, which pin is used?Thanks

Resolved! Datasheet for SPC58EC80E1

Posted on March 02, 2017 at 14:27Hello,I am working with the SPC58EC80E1 and cannot find a datasheet for this product.Most urgently, I would like the pin out of the device in TQFP64.Can anyone point to where I could get this?Thanks,Andrew