Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC560P ADC value not updating

Posted on July 12, 2017 at 10:30 Hello, I am workin on SPC560P Discovery Board. I am trying to initialize the ADCperipheral using the components provided in the SPC5 Studio. What I am trying to do is to replicate the ADC Test Application in a ...

Resolved! i have a problem of DSPI

Posted on June 29, 2017 at 11:40I use SPC5604B54L5 DSPI module, LTC6804 (Battery voltage acquisition chip) and the microcontroller through the SPI communication, the mode is CPOL = 1, CPHA = 1, but the communication is error.Before I used STM32 and ...

0690X00000607VVQAY.png 0690X00000607YJQAY.png

Hightec compiler problem with SPC5Studio

Posted on June 27, 2017 at 15:06Hello everyone,I have a problem with the Hightech compiler used in SPC5Studio, I try to explain my issue: on my PC I have installed the SPC5Studio v5.0.0 and the Hightec compiler toolchain v4.6.6.1.I configured the SP...

0690X00000607WcQAI.png

Resolved! i have two SPC5 I2C Driver problem and The SPC5studio IDE problem

Posted on June 26, 2017 at 11:46question 1:i2c_result_t i2c_lld_write(uint8_t dev_addr, uint16_t reg_addr,uint8_t *data, uint8_t ndata_bytes){..................  /* Check for valid address */   if ((dev_addr < 8U) || (dev_addr > 119U))    {      r...

SPI - spikes on the MOSI line between frames

Posted on May 03, 2017 at 18:05Hi, I am using the SPC570S40E1 microcontroller. When looking at the MOSI line on the scope, I am seeing spikes right around the end of a frame even when transmitting all zeros. The device I am trying to communicate wit...

Resolved! SPC560B-Discovery Schematics

Posted on March 23, 2017 at 14:57Hi,I am using SPC560B-Discovery EVK Board,I am facing some issue in input power can you please share the schematics of SPC560b-Discovery board,then it will be easy to me to debug the issue.---Thanks & Regards,Mujeeb 

Unable to Jump from Application to Boot loader

Posted on April 03, 2017 at 09:42Hello All,I am working with two different applications - boot loader application and main application together. The bootloader size is limited to 64k and the main application start address  changed to 64K. The jump t...

0690X00000606gvQAA.png

Cant get CAN to work on SPC56xL Discovery + board

Posted on May 09, 2014 at 14:46Appart from the fact that there are no specific examples for it, i have tried to do something with spc56ELxx OSLess CAN example from another board, and even though leds blink, there is no CAN data generated. I would re...

brd_gsm by Associate
  • 2825 Views
  • 9 replies
  • 0 kudos

SPC5Studio SPC570S MCU Wizard

Posted on March 17, 2017 at 07:57Hello Together,I am fairly new to developing Software using SPC5 Studio. I have been at the Embedded World and got an introduction to SPC5Studio. Unfortunately, I am unable to replicate what I have seen at the fair.C...

MD5 calculation of hex file

Posted on March 22, 2017 at 10:36Hi All,Is it possible to calculate the MD5 checksum of Hex file or elf using in SPC studio,If yes please let me know the procedure to calculate the MD5.Thanks in advance,---Thanks & Regards,Mujeeb