2020-11-02 4:19 AM
Hello, pin map editor is buggy for pins 88/89 of SPC564A80L7 and set always these pins as CAN and not eSCI when the pin map editor is opened and closed, code is generated as CAN!
I have modified thse pins function then directly in the code.
Thanks for your attention,
Best regards.
Solved! Go to Solution.
2020-11-02 5:55 AM
Hello ,
generated code is in board.c
No issue happened on SPC5Studio 5.8.1+ and 6.0
{(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE_PRIMARY)},
{(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE_PRIMARY)},
{(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE(2))},
{(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE(2))},Do not forget to save the configuration editor after saving and closing the pinmap editor ?
Could you send me your installation details ?
Best regards
Erwan
2020-11-02 5:55 AM
Hello ,
generated code is in board.c
No issue happened on SPC5Studio 5.8.1+ and 6.0
{(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE_PRIMARY)},
{(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE_PRIMARY)},
{(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE(2))},
{(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE(2))},Do not forget to save the configuration editor after saving and closing the pinmap editor ?
Could you send me your installation details ?
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.