Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Missing pal_lld.h in MCTK Lib on SPC5 Studio 6.0.0

Good day,I might be missing something, but an issue cropped up when I moved to SPC5 Studio 6.0.0 Asimov when attempting to compile any project that includes the MCTK Web Library. The message that I get while building is:./components/spc56xx_web_motor...

PMoll.1 by Associate
  • 1580 Views
  • 1 replies
  • 0 kudos

Resolved! About the PWM minimum duty cycle time in SPC58EC

Hello!​I have a SPC58EC-DISP; I set the PWM frequency 20KHz and duty cycle 1%,then it's not output,when set 8%,it's output 2us time;I found that the minimum PWM output time seems to be 2us.now I want PWM frequency 20KHz(50us) and 1%(0.5us) ouput,wh...

SLEE.6 by Associate II
  • 1990 Views
  • 2 replies
  • 0 kudos

Resolved! CAN setup in SPC570S-DISP dev board

Hi,I am trying to setup CAN communication in the SPC570S-DISP dev board. I started with the example available in the SPC5Studio. In the example, internal loopback is enabled, so I disabled it to allow external transmit. I did not change any other set...

0693W000006H6quQAC.png 0693W000006H6mUQAS.png 0693W000006H6slQAC.png
NBula.1 by Associate III
  • 2247 Views
  • 4 replies
  • 3 kudos

Resolved! Flash test application and bootloader for SPC584B70E5 discovery

Hi, Can someone guide me on where I can find the sample Flash test application and bootloader application for SPC584B70E5 discovery.I searched in import wizard of spcStudio but didnt find any.Thanks in advance. Flash test applications are available f...

CJadh by Associate II
  • 1990 Views
  • 3 replies
  • 0 kudos