AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem in executing the aek-pow bmslv demo fle

I have a problem when I try to follow the demo procedure step by step to test if the aek pow board reads the battery pack. I wanted to ask how I can solve this and I would like to know how to understand if the board has correctly gone into debug mode...

antonio0101_0-1757431263555.png antonio0101_1-1757431285376.png

Resolved! Cannot access About:Energy with ST battery models

Dear Experts, I cannot access the battery models from About:Energy with ST. I clicked Download model from Autodevkit Studio but the link said 404 page not found with the link: https://www.aboutenergy.io/stmicroelectronics-model-download. I also acces...

trishuynh_1-1757088233940.png trishuynh_0-1757088192774.png
trishuynh by Associate III
  • 2532 Views
  • 1 replies
  • 0 kudos

Resolved! How properly connect multiple L9963E in daisy chain

how to properly connect multiple L9963E in daisy chain? already tried many mode and tweak. follow the design in datasheet, for transformer isolated and capacitive, but still unable to init. for the first chip, I use SPI. init the first chip is correc...

jmary by Associate III
  • 1768 Views
  • 3 replies
  • 0 kudos

Resolved! AEK-COM-ISOSPI1 L9963T MISO and clock out of sync

Greetings I have weird situation with AEK-COM-ISOSPI1 and cannot figure out what is wrong. Maybe someone here is experienced with this device and can help me out. I have absolute encoder with SPI. When i connect directly to uC all is working fine. Th...

Frank2201 by Associate III
  • 8803 Views
  • 20 replies
  • 5 kudos

Resolved! make: ppc-freevle-eabi-gcc: No such file or directory

Hi,I'm trying to build SPC5 application in VS Studio Code on an agent environment (Windows), which does not have any installed SPC5Studio with Autodevkit plugin. The intention is to start a pipeline on AzureDevOps, where the project can be compiled a...

SD9_0-1713321713237.png
SD9 by Associate II
  • 4935 Views
  • 5 replies
  • 3 kudos

Resolved! User ADC, VBUS and NTC in AutoDevKit Studio

Dear ST team,Currently, I'm testing SPC560P50L5 MCU with AutoDevKit Studio, and it is going well by importing the sample project. I have noticed that I can enable "User ADC Regular Conversions" in "Application Configuration." Now, I'm trying to contr...

Agga by Associate II
  • 835 Views
  • 3 replies
  • 0 kudos

Resolved! SPC582B MCU - AEKS-MCU-SPC5LNKU - Debug issue

We are currently using the AEKS MCU-SPC5 LNKU Kit to debug our custom board. However, we are encountering a "launching error" when attempting to connect to the board via SPC5 Studio. For your reference, we have attached the error image below.We would...

Manikandaprabhu_0-1753422155758.png