AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where is the path of the spc5studio header file

Why can't I include the system standard header files? Why can I generate files even if there are problems as long as the console is fine when compiling? Finally, I can burn the program into the chip and run it successfully.

0693W00000WKWlRQAX.png 0693W00000WKWlHQAX.png 0693W00000WKWl2QAH.png 0693W00000WKWkxQAH.png
WMa.2 by Associate II
  • 1751 Views
  • 1 replies
  • 0 kudos

Resolved! hi im working on FDA903D AEK AUD D903V1 autodevkit, im trying to send information from an NXP MPCU5748G microcontroller through I2C AND I2S.

i have set enables 1,2,3 and 4 as 1100 which is address 2 , but for some reason the speaker is not open and voltage is not passing through it which means i cant move on and give orders through i2c registers, can you please explain what the reason mig...

aturk.2 by Associate II
  • 7960 Views
  • 18 replies
  • 0 kudos

Resolved! Is the board important for the AVAS project?

Hi, i have a AEK-AUD-D903V1 evaluation board and i want to make a simple AVAS project. I don't have any board with SPC582Bx microcontroller board. Can I implement this application to stm32 board ? if i can, how should i progress ?

aozba.1 by Associate II
  • 3573 Views
  • 6 replies
  • 0 kudos

Resolved! PUSH BUTTON

May i know in what library used for push button or the example code for push button?

Angle by Associate II
  • 2300 Views
  • 3 replies
  • 0 kudos

www.st.com

Have you already downloaded the latest AutoDevKit release 1.6.0?www.st.com/autodevkitsw#transportation #automotive #embeddedsoftware #engineering#keepdreaming

Resolved! Serial DMA buffer position

Hi,I am developing an application on SPC58EC that uses the serial with DMA for reading.I'd like to know if there is a way to know and get the position where it's writing in the buffer. I mean something like the corresponding "__HAL_DMA_GET_COUNTER(.....

RD'Ig by Associate II
  • 2440 Views
  • 2 replies
  • 0 kudos

lnkd.in

Fully deployed with mobile phone Android and iOS APP, web application and Windows desktop application, AEK EXPLORER is now your best companion to discover AutoDevKit ecosystem and generate projects on the fly!Mobile APPs - STSW-AEKEXPLORER https://ln...

0693W00000FCQUQQA5.png