AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Adding breakpoint and debugging using UDE STK 2021

Hello everyone,I have been flashing the code written in AutDevKit Studio 2.4.0 using UDE STK 2021 for the AEK-AUD-C1D9031, which uses the SPC582B60E1 MCU. I want to start debugging the code line by line using breakpoints.Currently, I have the option ...

Resolved! How to read initialization from L9663 data using SPI?

Hello, I stareted to develop PSI5 interface with L9663. My point is to read initialization data via SPI. If I set DOUT1 as direct data output (CH1_CR1->DOUT1_SE = 0), I am able to measure received data on this pin. But if  I set this pin as interrupt...

Ondrej1_0-1707316125721.png
Ondrej1 by Associate II
  • 5067 Views
  • 7 replies
  • 0 kudos

Resolved! VN9D5F20F SPI error problem

Hi everyone,I am implementing the communication between MCU SPC582B and High side driver VN9D5D20F. SPI signals seem fine to me, see next image:Spi Clk frequency = 625kHz  (range is 0Mhz to 8Mhz)CS transaction time = 71usTime between bytes = 7usTrans...

FPros1_0-1707317718252.png
FPros.1 by Associate III
  • 2830 Views
  • 3 replies
  • 0 kudos

Resolved! Issue rised during flasing and debugging

Hello Team,I hope this message finds you well.I am reaching out to seek your guidance regarding an issue I am encountering while flashing software. Despite following the standard procedures, I am facing the following errors (as shown in the attached ...

Aishwaryaum_1-1736424682036.jpeg Aishwaryaum_2-1736424690531.jpeg

Resolved! AEK-POW_BMS63EN cell balancing manually adjust

Dear community members, There are multiple functions related to cell balancing in AEK-POW_BMS63EN_id. However, when I tested, none of them work. Here is my main code based on the "SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_14Cells_GUI application for d...

trishuynh_0-1730455880757.png trishuynh_1-1730455908832.png
trishuynh by Associate III
  • 16675 Views
  • 12 replies
  • 0 kudos

Resolved! L9963E Burst frame response error

Dear Community member,In L9963E burst response for 0x78, we are getting only 17 response frames out of 18 after feedback response.Last frame 18 is missing. Also the cell 7,8,9,10 is disable, while it is showing no data(for disable cell) for cell 6,7,...

bitBuddy by Associate II
  • 2462 Views
  • 2 replies
  • 0 kudos

Resolved! AEK_POW_BMS63EN Fault_L_line_status is always 1

Dear Community members,I have connected 2 node in ring configuration, and working on an custom pcb for BMS.In registers Faults1, Fault_L_line_status is always 1, while all other fields of Faults1 and Faults2 registers are 0. Also the OVRLATCH is not ...

bitBuddy by Associate II
  • 4950 Views
  • 6 replies
  • 1 kudos