AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AEK-POW_BMS63EN : Fault pin is not being high

Dear Community members,In an SPC582b-discovery example code, i modified configuration to set over voltage threshold 3.4 v. While all the cells in stack is over than 3.4 but the Fault pin in board is not being high.  Regards,bitBuddy

bitBuddy by Associate II
  • 2281 Views
  • 1 replies
  • 0 kudos

Resolved! L9963E meaning of VTREF_BIST_FAIL flag

Hi,The screenshot below is from the L9963E datasheet DS13636, page 125. Is the description for VTREF_BIST_FAIL here a typo?It matches exactly the description of a the VCOM_COMP_BIST_FAIL bit in the BIST_COMP register, which makes more sense. I note t...

abtjmehmet_0-1726654040604.png

Resolved! Regarding sound optimization in AVAS

Hello all,A very good morning, I hope you all have the good day.I am developing the AVAS project taking the base code(shown in the snippet) from the AutoDevKit.Here my requirement is I need to increase the sound from speed 0 to 20kmph and sound shoul...

Aishwaryaum_0-1727416129427.png

Resolved! Issue downloading free license for Hightech Compiler

Hi everyone,I’m trying to download a free license for the Hightech compiler from the following link:https://register.hightec-rt.com/st/spc5x/Unfortunately, the page returns the following error:This page isn’t workingThe site register.hightec-rt.com i...

Mjuchelka by Associate II
  • 2625 Views
  • 2 replies
  • 0 kudos

Resolved! AutoDevKitStudio Pin Map generation

Hi,I have recently started working with AutoDevKitStudio and tried some of the example codes. When I wanted to modify example code and add more pins in Pin Map editor, after saving my changes and generating them I couldn't see newly defined ports in ...

MaraLo by Associate II
  • 2454 Views
  • 3 replies
  • 0 kudos

AVAS - how to load an audio file with OpenOCD

#autodevkit hashtag#avas hashtag#openocd hashtag#mcu hashtag#spc5 hashtag#embedded hashtag#automotiveHere you are a quick guide to help you load the audio file in AEK-AUD-C1D9031 Avas board using the AEK-MCU-SPC5LNK programmer.AEK-AUD-C1D9031 - https...