2021-04-16 9:04 AM
Dears, Good morning.
Regarding TDA7419's spectrum analyzer, the datasheet says:
"A reset of the sample capacitors is induced whenever SAclk remains high for the time tintres" From the tables, Tintres is 3ms.
Question: Is there a way to partially discharge the sample capacitor? I would like, for example, do 10 reads and for each one obtain decay of 10%. Maybe if I do each SAclk high for 300us (1/10 of Tintres) I can achieve this behavior for each reading cycle.
Thank you very much,
Leonardo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.