Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Resolved! Comparator with Hysteresis_Design Calculations

I need to design a comparator with Vih=1.3V and Vil=1.2V. Therefore hysteresis is 100mV. The circuit will be working on a 3.3V supply. During high state, the o/p of the comparator will be 3.3V and at the low state, it will be 0V. I will be using a co...

HT O.1 by Associate
  • 3198 Views
  • 3 replies
  • 0 kudos

目�?�?用的LM358芯片,�?�电压跟�?器,出现输入电压V+为0V时输出电压有�??几�?

现在有一个项目上用了LM358�?放,�?�电压跟�?器用,用在电机上的,现在出现的问题如下:358是15V供电�?�了一百多�?��?��?,有差�?多五六个出现了下述情况,�?良的芯片输入电压V+为0V时输出电压有�??几�?,�?良的芯片正常工作时,输出电压�?�是正常的,�?�是输入电压是多少输出电压就是多少。项目比较急,麻烦尽快帮分�?下原因​原�?�图如下:​

0693W00000AM4ojQAD.png
QLiu.2 by Associate
  • 762 Views
  • 1 replies
  • 0 kudos

How to partially discharge TDA7419 spectrum analyzer capacitors?

Dears, Good morning.Regarding TDA7419's spectrum analyzer, the datasheet says:"A reset of the sample capacitors is induced whenever SAclk remains high for the time tintres" From the tables, Tintres is 3ms.Question: Is there a way to partially dischar...

LCabr.3 by Associate
  • 721 Views
  • 0 replies
  • 0 kudos

TS4909 - high white noise output

Hi all!I've been strugling with this TS4909 for 2 weeks now, and cannot get it work properly...I've designed a custom application with TS4909 as audio amp.The problem is is has high white noise on the output.My power supply is clean (from LDO), no no...

AMart.11 by Associate
  • 940 Views
  • 1 replies
  • 0 kudos

STA350BW delay

Hello everyone,I'm working on nucleo-f446re and x-nucleo-cca01m1 demoboard, using last version of FP-AUD-SMARTMIC1 software.The STM32F4 sends audio data to two speakers through the STA350BW via I2S interface.The output sampling frequency is 32kHz. I2...

0693W000008yD1iQAE.png
MRivo.1 by Associate
  • 945 Views
  • 0 replies
  • 0 kudos