Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Correcting Phase of STA311b System with speaker response?

Posted on November 24, 2014 at 12:52Hello, I built a system using a ad converter (PCM4202 from TI) and a sta311b DSP. I drive the power fets with the ffx pwm stage of the sta311b. When I measure the phase response of the hole system (without any dsp...

Difference between LM224 and LM224A

Posted on November 28, 2014 at 09:04Hi, Is there tmeperature drift difference between the two types? Or is there any other difference between the two type,please? Thanks!

STSpeakerTune for automatic loudspeaker compensation

Posted on November 25, 2014 at 12:16As the STSpeakerTune technology is now freely available in the latest APWorkbench v2.1.0 here's a quick step-through list to assess the feature: Run APWorkbench (download it from http://www.st.com/apworkbench an...

ESM7045DV datasheets

Posted on November 09, 2014 at 03:48Dear all, I had been trying really very hard to search by internet and or trying to call ST distributor searching for DATASHEETS of ESM7045DV, unfortunately I found nothing.  Is there anyone that could help me out...

hongya_li by Associate II
  • 1916 Views
  • 3 replies
  • 0 kudos

DDX and FFX

Posted on November 10, 2014 at 01:20Hi     I try to add an external amplifier to STA350BW, the external amplifier work as subwoofer,but I realize that there are two type amplifiers: STA510A(DDX output)and STA510F(FFX output), I can't find any inform...

DDX and FFX

Posted on November 07, 2014 at 07:59hello     I try to connect an external amplifier to STA350BW, the external amplifier work as subwoofer,but I realize that there are two amplifiers STA510A(DDX output)and STA510F(FFX output), I can't find any infor...

331912674 by Associate II
  • 1099 Views
  • 2 replies
  • 0 kudos

STA333 and APW questions...

Posted on July 20, 2014 at 18:04Hello, first : can i use STA333 with filterless output (only snubber) ? (and sound quality ...better , than with filter ?) and in the APW gui, i cannot import speaker response (F5) - not working; is this only working,...

alfsch by Associate II
  • 1482 Views
  • 4 replies
  • 0 kudos

MKI138V1 (STAudioHub) not communicating with APWorkbench

Posted on July 07, 2014 at 15:32Hello.If I connect the board to my computer it recognizes it and installs some drivers.It will after that show up as a ''STM Device in DFU Mode'' under USB controllers in the device manager. But in the APWorkbench the...

robin by Associate
  • 1121 Views
  • 3 replies
  • 0 kudos