2014-11-09 4:20 PM
Hi
I try to add an external amplifier to STA350BW, the external amplifier work as subwoofer,but I realize that there are two type amplifiers: STA510A(DDX output)and STA510F(FFX output), I can't find any information about this two mode。 my question is:STA350BW must work with FFX amplifier?or both DDX and FFX amplifier?
2014-11-09 7:53 PM
hi Karl,
STA350BW can work with both DDX and FFX amplifier . you need to set OCFG bits to 10 for this configuration . ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.