2014-11-28 12:04 AM
Hi,
Is there tmeperature drift difference between the two types? Or is there any other difference between the two type,please? Thanks!2014-11-28 2:38 AM
Hi wang.zhen.003,
For most of ST operational amplifier product the A label define a product with a better Vio.
You don’t have any difference one the DVio/DT = 7µV/°C in typical value or 30µV/°C for max value in the both cases.
If you compare the max Vio value between LM224 and LM224A you can see a difference of 2mV.
Ambient:5mV -> 3mV(A version)
Temperature:
7mV -> 5mV(A version)
Regards
Florian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.