Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

5 samples latency on STA321MPL?

Posted on October 13, 2016 at 04:50My SW read audio with PCM format from STA321MPL. The same time it read PDM format from Digital Microphone. Both are set with 16 Khz sample rate. It always has5 samples delay in audio signal from STA321MPL compare t...

son1 by Associate II
  • 1011 Views
  • 1 replies
  • 0 kudos

Choosing the right amplifier

Posted on September 22, 2016 at 15:22I'm planning to make a speaker system, and need the right amplifier ic. The input have to be I2S and the amp is going to power four 8 ohms drivers with 50W max. Should I go with a single ic to power all four driv...

trym1994 by Associate
  • 641 Views
  • 0 replies
  • 0 kudos

STA311B reference design schematic

Posted on August 28, 2016 at 03:54Hello, I cannot find the typical  application design schematic for STA311B, can you please send me one? thanks. David.

lds330 by Associate
  • 897 Views
  • 1 replies
  • 0 kudos

TDA7498

Posted on September 09, 2016 at 12:58Hi ST.  I have a few questions regarding the application of the TDA7498 and TDA7498E.The TDA7498E application circuit has schottky diodes on the output but the TDA7498 does not, is there a reason for this?The lou...

mc2 by Associate
  • 1113 Views
  • 1 replies
  • 0 kudos

TSC101 connection question

Posted on July 18, 2016 at 08:34Hello there, I have a question regarding TSC101 amplifier. Will it work if current will flow through the sense resistor in a reverse direction? I was wondering either it is possible to use it like this:https://dl.drop...

about TDA7492P burn

Posted on August 10, 2016 at 18:11hi,    I had some questions when i use the TDA7492P. When I turn on the 12V power(connect to the PVCC)and don't connect the 5V(connect to the SVCC), the pin1 of TDA7492P will immediately burn( the pin1 will short wi...

STA321MP INQUIRIES

Posted on July 09, 2016 at 02:05Greetings, currently i am working on my thesis and i am planning to use this IC (STA321MP) for my proyect as it fits the requierments that i am proposing for it, but there are some specific points and doubts that i ca...

0690X00000604xkQAA.png 0690X00000604joQAA.png
carsacc by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

TSX711ILT FIT Reliability Data

Posted on June 21, 2016 at 18:44Hi,I am looking for the FIT data and test conditions for part number TSX711ILT. I could not find the information available on the website.

TDA-7498-L burn

Posted on June 28, 2016 at 16:01Hi To all, I have a problem to new design, based to de datasheet of the TDA-7498-L, Every time when I put in STBY off, the Intensity increase, and the device is burn. I compare two, diagrams and I doesn�t found possib...

avionica by Associate
  • 2074 Views
  • 3 replies
  • 0 kudos

TSX564 quad OP with QFN package NC pins

Posted on June 16, 2016 at 15:26Hi guys! I�am currently working on a sensor hardware. I use the TSX564 quad CMOS operational amplifiers with the QFN16 package. There are two pins called NC. So does it means they are Not Connected with a bond to the ...

tknobloc by Associate
  • 919 Views
  • 1 replies
  • 0 kudos