2019-05-29 6:48 PM
When STM32CubeProgrammer first connects to my STM32F7779I-EVAL board, it fails to read the QSPI Flash. All Flash memory appears as '0's. Loading and unloading the external loader (MT25QL512A_STM32769I-EVAL) makes no difference. If I erase an arbitrary unused sector, I can then read the rest of the Flash successfully.
I'm experiencing different issues with my own Flash driver. In my case after I have programmed the board, I have to power cycle the board before I can read the QSPI Flash.
Is anyone else experiencing this issue? Could there be a compatibility issue with STM32F769I and STM32F779I?
Cheers,
David
Solved! Go to Solution.
2019-05-30 6:09 AM
Low pin count devices often lack an explicit reset pin and mux it with other functionality. It might be necessary to retry READ ID or similar commands, or try recovery when the device comes up in an indeterminate state. The docs might provide specific guidelines.
2019-05-30 6:09 AM
Low pin count devices often lack an explicit reset pin and mux it with other functionality. It might be necessary to retry READ ID or similar commands, or try recovery when the device comes up in an indeterminate state. The docs might provide specific guidelines.
2019-06-01 7:17 PM
Yes, you're right. I checked the schematic and the reset line doesn't go to the Flash chip. I'll look into alternate ways of resetting it.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.