2024-11-12 11:52 PM
Hi
I have designed a header board for the STM32H562RIT6 microcontroller, but no matter how hard I try, I can't program it! The wiring is as follows. Please guide me on how to program this microcontroller. If there are any tips or specific instructions for programming this microcontroller, I would appreciate your help.
WIRING ( SIMILAR TO AN5711 PAGE 36 ) :
All VDD and VDDA pins → connect to 3.3V
All VSS and VSSA pins → connect to GND
BOOT0 → connect to GND through a 10kΩ resistor
RESET → connect to GND through a 100nF capacitor
Connect the two VCAP pins together, and connect each pin to a 2.2µF capacitor
PROGRAMMER : ST-LINK V2 ( 3.3V , GND , SWDIO , SWCLK )
Solved! Go to Solution.
2024-11-13 1:52 AM - edited 2024-11-13 2:00 AM
Hello,
@Farhad13651 wrote:
The software is STM32 ST-LINK Utility, and I have placed Roshamatic in the "Youst" folder.
No. ST-LINK Utility is an old tool and doesn't support that device. You need to use STM32CubeProgrammer instead.
2024-11-13 12:51 AM
Hello @Farhad13651 and welcome to the community,
1- Insufficient information. Better to share your schematics.
2- What tools are you using? STLINK (genuine or not) with STM32CubeProgrammer or CubeIDE?
2024-11-13 1:50 AM - edited 2024-11-13 2:01 AM
2024-11-13 1:51 AM
2024-11-13 1:52 AM - edited 2024-11-13 2:00 AM
Hello,
@Farhad13651 wrote:
The software is STM32 ST-LINK Utility, and I have placed Roshamatic in the "Youst" folder.
No. ST-LINK Utility is an old tool and doesn't support that device. You need to use STM32CubeProgrammer instead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.