2022-03-31 9:45 AM
Hi all. I am using STM32CubeProgrammer with an STM32G474VET6 target system on a Windows 10 box with a USB-connected STLink module. The programmer is v2.10.0, and the STL firmware is v2J3757.
My problem is that the Cube programmer doesn't seem to be able to perform a mass erase on the target prior to programming. When I try to program, I get the following message:
Error: failed to erase memory
The Full chip erase button fails as well with
Error: Mass erase operation failed.Please verify flash protection
Flash write protection is not enabled on the target. I can erase and program just fine with the STM32 ST-LINK Utility. Also, Cube programs successfully if the target device flash is blank.
I'm happy to provide any of the target settings on request.
Any ideas?
Thanks,
Mike
2022-03-31 10:14 AM
More info - I set the output verbosity level to 3 (highest) and harvested the following:
11:43:44:651 : MASS ERASE ...
11:43:44:652 : Flash erase...
11:43:44:655 : halt ap 0
11:43:44:655 : w ap 0 reg 15 PC (0x20000000)
11:43:44:657 : w ap 0 reg 17 MSP (0x20000500)
11:43:44:657 : w ap 0 reg 16 xPSR (0x01000000)
11:43:44:667 : w ap 0 @0x20000C80 0x00000200 bytes Data 0x00000000
11:43:44:668 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
11:43:44:681 : w ap 0 @0x20000004 0x00000848 bytes Data 0xB672B580
11:43:44:681 : Init flashloader...
11:43:44:681 : halt ap 0
11:43:44:681 : w ap 0 reg 0 R0 0x00000001
11:43:44:681 : w ap 0 reg 1 R1 0x00000000
11:43:44:681 : w ap 0 reg 2 R2 0x00000000
11:43:44:682 : w ap 0 reg 3 R3 0x00000000
11:43:44:682 : w ap 0 reg 4 R4 0x00000000
11:43:44:682 : w ap 0 reg 5 R5 0x00000000
11:43:44:683 : w ap 0 reg 6 R6 0x00000000
11:43:44:683 : w ap 0 reg 7 R7 0x00000000
11:43:44:683 : w ap 0 reg 8 R8 0x00000000
11:43:44:683 : w ap 0 reg 9 R9 0x00000000
11:43:44:686 : w ap 0 reg 10 R10 0x00000000
11:43:44:688 : w ap 0 reg 11 R11 0x00000000
11:43:44:688 : w ap 0 reg 12 R12 0x00000000
11:43:44:689 : w ap 0 reg 13 SP 0x00000000
11:43:44:690 : w ap 0 reg 14 LR 0x20000001
11:43:44:690 : w ap 0 reg 15 PC 0x20000005
11:43:44:690 : w ap 0 reg 16 xPSR 0x01000000
11:43:44:691 : w ap 0 reg 17 MSP 0x20000C48
11:43:44:691 : w ap 0 reg 18 PSP 0x00000000
11:43:44:691 : run ap 0
11:43:45:648 : halt ap 0
11:43:45:648 : r ap 0 reg 0 R0 0x00000001
11:43:45:648 : Loader mass erase...
11:43:45:648 : Error: Mass erase operation failed.Please verify flash protection
2022-04-06 1:04 PM
Hello @SDiMo.1 ,
Did you try to connect under reset?
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.