2025-07-02 10:31 PM - last edited on 2025-07-03 7:28 AM by Andrew Neil
Hello,
I'm encountering a connection error with STM32CubeProgrammer when trying to connect to my NUCLEO-H7A3ZI-Q board.
**Error Details:**
- Error: "No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"
- Board: NUCLEO-H7A3ZI-Q
- STM32CubeProgrammer version: v2.19.0
- OS: Windows 64-bit
- ST-LINK SN: 001C004330325115373336
- ST-LINK FW: V3J15M7
- Board Voltage: 1.22V
**What I've tried:**
- Checked USB cable connection
- Verified ST-LINK drivers installation
- Tried different USB ports
- Board appears to be detected (shows serial number and firmware)
**Question:**
How can I resolve this "No STM32 target found" error? Is the 1.22V voltage reading normal, or could this indicate a power issue?
Any help would be greatly appreciated!
Best regards
Solved! Go to Solution.
2025-07-03 7:25 AM - edited 2025-07-03 7:27 AM
@patelshre_21 wrote:- Board appears to be detected (shows serial number and firmware)
Indeed, but that's just the connection from the PC to the ST-Link.
So the problem is somewhere beyond the ST-Link ...
How to solve connection errors when connecting and programming the STM32 target board.
How to solve debugger connection issues
Unable to connect to STM32H7 devices
How can I recover my STM32H7/STM32H7RS board after facing a power configuration deadlock?
2025-07-03 6:59 AM
1.22 V is insufficient power. The ST-Link chip appears okay since it is detected, but the STM32H7 chip appears to have insufficient power. Download the schematic and trace power on the board to see what is damaged and fix it.
2025-07-03 7:22 AM
@TDK wrote:Download the schematic and trace power on the board to see what is damaged and fix it.
Could also be a misconfiguration? The board has several powering options ...
@patelshre_21 Check in the User Manual and/or the schematics that you have the board correctly configured
2025-07-03 7:25 AM - edited 2025-07-03 7:27 AM
@patelshre_21 wrote:- Board appears to be detected (shows serial number and firmware)
Indeed, but that's just the connection from the PC to the ST-Link.
So the problem is somewhere beyond the ST-Link ...
How to solve connection errors when connecting and programming the STM32 target board.
How to solve debugger connection issues
Unable to connect to STM32H7 devices
How can I recover my STM32H7/STM32H7RS board after facing a power configuration deadlock?
2025-08-04 10:17 PM
thank you very much but board was faulty i return to supplier they sent me new one.
2025-08-04 10:17 PM
yes you are correct , thank you very much.
2025-08-05 1:26 AM
Good to hear. Now please mark the solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.