2019-10-17 12:11 AM
Hi there,
I have 5 STM32F769I-DISCO connected to a Linux PC.
They do all show up using lsusb:
Bus 002 Device 012: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC
Bus 002 Device 010: ID 2109:2811 VIA Labs, Inc. Hub
Bus 002 Device 008: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
Bus 002 Device 006: ID 0483:374b STMicroelectronics ST-LINK/V2.1 (Nucleo-F103RB)
Bus 002 Device 004: ID 2109:2811 VIA Labs, Inc. Hub
Bus 002 Device 013: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC
Bus 002 Device 011: ID 0483:374b STMicroelectronics ST-LINK/V2.1 (Nucleo-F103RB)
Bus 002 Device 009: ID 2109:2811 VIA Labs, Inc. Hub
Bus 002 Device 007: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
Bus 002 Device 005: ID 0483:374b STMicroelectronics ST-LINK/V2.1 (Nucleo-F103RB)
Bus 002 Device 003: ID 2109:2811 VIA Labs, Inc. Hub
Bus 002 Device 002: ID 8087:8000 Intel Corp.
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 010: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC
Bus 001 Device 009: ID 0483:374b STMicroelectronics ST-LINK/V2.1 (Nucleo-F103RB)
Bus 001 Device 008: ID 2109:2811 VIA Labs, Inc. Hub
Bus 001 Device 007: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
Bus 001 Device 006: ID 0483:374b STMicroelectronics ST-LINK/V2.1 (Nucleo-F103RB)
Bus 001 Device 005: ID 2109:2811 VIA Labs, Inc. Hub
Bus 001 Device 004: ID 03f0:304a Hewlett-Packard
Bus 001 Device 003: ID 046d:c063 Logitech, Inc. DELL Laser Mouse
Bus 001 Device 002: ID 8087:8008 Intel Corp.
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hubExecuting "STM32_Programmer_CLI -l -vb 3" list only four of them:
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== STLink Interface =====
STLinkUSBDriver.dll loaded
STLinkUSBDriver.dll loaded
STLinkUSBDriver.dll loaded
STLinkUSBDriver.dll loaded
-------- Connected ST-LINK Probes List --------
ST-Link Probe 0 :
ST-LINK SN : 066EFF575251717867105346
ST-LINK FW : V2J29M18
ST-Link Probe 1 :
ST-LINK SN : 0672FF343636574D43044450
ST-LINK FW : V2J29M18
ST-Link Probe 2 :
ST-LINK SN : 066CFF575251717867114129
ST-LINK FW : V2J29M18
ST-Link Probe 3 :
ST-LINK SN : 066BFF575251717867114126
ST-LINK FW : V2J29M18
-----------------------------------------------There will be 6 boards in the final setup. Is there a limitation in STM32CubeProgrammer regarding the number of probes?
Kind regards,
Wolfram
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.