2025-02-13 10:21 PM
Hi to all
I just wan't to use the CLI inteface from STM32CubeProgrammer and I don't want to installl the full SMT32CubeProgrammer which is about 1.3GB.
Is there a Standalone Version from the STM32CubeProgrammer CLI?
Best regards
2025-02-13 10:28 PM
2025-02-14 6:36 AM
There's not a standalone unfortunately, and STM32CubeProgrammer has grown to be a beast. We used to have the relatively lightweight ST-Link Utility, which still works for older chips.
There is the open source st-flash which mostly works but can struggle with newer hardware until development catches up.
stlink-org/stlink: Open source STM32 MCU programming toolset
Think those are your only options.
2025-02-14 6:58 AM - edited 2025-02-14 6:58 AM
CubeProgrammer CLI is not just the program itself. (even with all these chubby Qt libraries). It comes with database of MCUs and external loaders. Bottom line: keep it simple, not small.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.