2019-02-22 1:18 AM
Hi,
I've developed an external loader for an external SPI flash.
My external loader has a Read() function.
In STM32 Cube Programmer version 1.4.0, I found that initializing of
the loader and reading of data are eternally repeated when verification
after programming. The log (verbosity level = 2) is as follows:
16:59:01:640 : Memory Programming ...
16:59:01:640 : Opening and parsing file: flash.axf
16:59:01:661 : File : flash.axf
16:59:01:661 : Size : 1016700 Bytes
16:59:01:661 : Address : 0x90000000
16:59:01:661 : Erasing memory corresponding to segment 0:
16:59:01:661 : Memory erase...
16:59:01:740 : Erasing external memory sectors [0 15]
16:59:01:740 : Init flashloader...
16:59:01:794 : Loader sector erase...
16:59:06:050 : Download in Progress:
16:59:06:050 : Size : 1016700 Bytes
16:59:06:050 : Address : 0x90000000
16:59:06:050 : Buffer program...
16:59:06:126 : Loader write range...
16:59:07:018 : Init flashloader...
16:59:13:878 : Segment[0] downloaded successfully
16:59:13:878 : File download complete
16:59:13:900 : Time elapsed during download operation: 00:00:12.217
16:59:13:901 : Verifying ...
16:59:13:903 : Read progress:
16:59:13:903 : Reading data...
16:59:13:955 : Loader read...
16:59:13:955 : Init flashloader...
16:59:14:026 : Reading data...
16:59:14:104 : Loader read...
16:59:14:104 : Init flashloader...
16:59:14:179 : Reading data...
16:59:14:260 : Loader read...
16:59:14:260 : Init flashloader...
16:59:14:336 : Reading data...
16:59:14:414 : Loader read...
16:59:14:415 : Init flashloader...
16:59:14:486 : Reading data...
16:59:14:564 : Loader read...
16:59:14:564 : Init flashloader...
16:59:14:637 : Reading data...
16:59:14:713 : Loader read...
16:59:14:713 : Init flashloader...
16:59:14:784 : Reading data...
...
When verbosity = 3, the log reports:
...
17:03:58:246 : Segment[0] downloaded successfully
17:03:58:246 : File download complete
17:03:58:267 : Time elapsed during download operation: 00:00:12.132
17:03:58:267 : Verifying ...
17:03:58:270 : Read progress:
17:03:58:270 : Reading data...
17:03:58:270 : reset ap 0
17:03:58:270 : run ap 0
17:03:58:270 : halt ap 0
17:03:58:270 : w ap 0 reg 15 (0x20000000)
17:03:58:270 : w ap 0 reg 17 (0x20000500)
17:03:58:270 : w ap 0 reg 16 (0x01000000)
17:03:58:270 : w ap 0 @0x20002BE0 0x00000200 bytes
17:03:58:270 : w ap 0 @0x20000000 0x00000004 bytes
17:03:58:270 : w ap 0 @0x20000004 0x000027A4 bytes
17:03:58:270 : Loader read...
17:03:58:270 : Init flashloader...
17:03:58:270 : halt ap 0
17:03:58:271 : w ap 0 reg 0 0x00000000
17:03:58:271 : w ap 0 reg 1 0x00000000
17:03:58:271 : w ap 0 reg 2 0x00000000
17:03:58:271 : w ap 0 reg 3 0x00000000
17:03:58:271 : w ap 0 reg 4 0x00000000
17:03:58:271 : w ap 0 reg 5 0x00000000
17:03:58:271 : w ap 0 reg 6 0x00000000
17:03:58:271 : w ap 0 reg 7 0x00000000
17:03:58:271 : w ap 0 reg 8 0x00000000
17:03:58:271 : w ap 0 reg 9 0x00000000
17:03:58:271 : w ap 0 reg 10 0x00000000
17:03:58:271 : w ap 0 reg 11 0x00000000
17:03:58:271 : w ap 0 reg 12 0x00000000
17:03:58:271 : w ap 0 reg 13 0x00000000
17:03:58:271 : w ap 0 reg 14 0x20000001
17:03:58:271 : w ap 0 reg 15 0x20000005
17:03:58:271 : w ap 0 reg 16 0x01000000
17:03:58:271 : w ap 0 reg 17 0x20002BA4
17:03:58:271 : w ap 0 reg 18 0x00000000
17:03:58:271 : run ap 0
17:03:58:558 : halt ap 0
17:03:58:558 : r ap 0 reg 0 0x00000001
17:03:58:558 : w ap 0 reg 0 0x90000000
17:03:58:558 : w ap 0 reg 1 0x00000400
17:03:58:558 : w ap 0 reg 2 0x20002BE0
17:03:58:558 : w ap 0 reg 3 0x00000000
17:03:58:558 : w ap 0 reg 4 0x00000000
17:03:58:558 : w ap 0 reg 5 0x00000000
17:03:58:558 : w ap 0 reg 6 0x00000000
17:03:58:558 : w ap 0 reg 7 0x00000000
17:03:58:558 : w ap 0 reg 8 0x00000000
17:03:58:558 : w ap 0 reg 9 0x00000000
17:03:58:558 : w ap 0 reg 10 0x00000000
17:03:58:558 : w ap 0 reg 11 0x00000000
17:03:58:559 : w ap 0 reg 12 0x00000000
17:03:58:559 : w ap 0 reg 13 0x00000000
17:03:58:559 : w ap 0 reg 14 0x20000001
17:03:58:559 : w ap 0 reg 15 0x2000193D
17:03:58:559 : w ap 0 reg 16 0x01000000
17:03:58:559 : w ap 0 reg 17 0x20002BA4
17:03:58:559 : w ap 0 reg 18 0x00000000
17:03:58:559 : run ap 0
17:03:58:559 : halt ap 0
17:03:58:570 : r ap 0 reg 0 0x00000001
17:03:58:960 : r ap 0 @0x20002BE0 0x00000400 bytes
17:03:58:960 : Reading data...
17:03:58:961 : reset ap 0
17:03:58:961 : run ap 0
17:03:58:961 : halt ap 0
17:03:58:961 : w ap 0 reg 15 (0x20000000)
17:03:58:961 : w ap 0 reg 17 (0x20000500)
17:03:58:961 : w ap 0 reg 16 (0x01000000)
17:03:58:961 : w ap 0 @0x20002BE0 0x00000200 bytes
17:03:58:961 : w ap 0 @0x20000000 0x00000004 bytes
17:03:58:961 : w ap 0 @0x20000004 0x000027A4 bytes
17:03:58:961 : Loader read...
17:03:58:961 : Init flashloader...
17:03:58:961 : halt ap 0
17:03:58:961 : w ap 0 reg 0 0x00000000
17:03:58:961 : w ap 0 reg 1 0x00000000
17:03:58:961 : w ap 0 reg 2 0x00000000
17:03:58:961 : w ap 0 reg 3 0x00000000
17:03:58:961 : w ap 0 reg 4 0x00000000
17:03:58:961 : w ap 0 reg 5 0x00000000
17:03:58:961 : w ap 0 reg 6 0x00000000
17:03:58:961 : w ap 0 reg 7 0x00000000
17:03:58:961 : w ap 0 reg 8 0x00000000
17:03:58:961 : w ap 0 reg 9 0x00000000
17:03:58:961 : w ap 0 reg 10 0x00000000
17:03:58:961 : w ap 0 reg 11 0x00000000
17:03:58:961 : w ap 0 reg 12 0x00000000
17:03:58:962 : w ap 0 reg 13 0x00000000
17:03:58:962 : w ap 0 reg 14 0x20000001
17:03:58:962 : w ap 0 reg 15 0x20000005
17:03:58:962 : w ap 0 reg 16 0x01000000
17:03:58:962 : w ap 0 reg 17 0x20002BA4
17:03:58:962 : w ap 0 reg 18 0x00000000
17:03:58:962 : run ap 0
17:03:58:962 : halt ap 0
17:03:58:962 : r ap 0 reg 0 0x00000001
17:03:58:962 : w ap 0 reg 0 0x90000000
17:03:58:962 : w ap 0 reg 1 0x00000400
17:03:58:962 : w ap 0 reg 2 0x20002BE0
17:03:58:962 : w ap 0 reg 3 0x00000000
17:03:58:962 : w ap 0 reg 4 0x00000000
17:03:58:962 : w ap 0 reg 5 0x00000000
17:03:58:962 : w ap 0 reg 6 0x00000000
17:03:58:962 : w ap 0 reg 7 0x00000000
17:03:58:962 : w ap 0 reg 8 0x00000000
17:03:58:962 : w ap 0 reg 9 0x00000000
17:03:58:962 : w ap 0 reg 10 0x00000000
17:03:58:962 : w ap 0 reg 11 0x00000000
17:03:58:962 : w ap 0 reg 12 0x00000000
17:03:58:962 : w ap 0 reg 13 0x00000000
17:03:58:962 : w ap 0 reg 14 0x20000001
17:03:58:962 : w ap 0 reg 15 0x2000193D
17:03:58:962 : w ap 0 reg 16 0x01000000
17:03:58:962 : w ap 0 reg 17 0x20002BA4
17:03:58:963 : w ap 0 reg 18 0x00000000
17:03:58:963 : run ap 0
17:03:58:963 : halt ap 0
17:03:58:963 : r ap 0 reg 0 0x00000001
17:03:58:963 : r ap 0 @0x20002BE0 0x00000400 bytes
17:03:58:963 : Reading data...
17:03:58:963 : reset ap 0
17:03:58:963 : run ap 0
17:03:58:963 : halt ap 0
17:03:58:963 : w ap 0 reg 15 (0x20000000)
...
where 0x20000005 and 0x2000193D are the addresses of the Init and Read
functions, respectively (I’ve checked the map file of my loader).
It seems that the loader was re-initialized although Read() successfully
returned 1.
I have no problem in ST-Link utility with the same executable of the
loader. In "Memory & File edition" of the STM32 Cube Programmer, I also
have no problem at reading data from the external flash.
I noticed that programming with verification successfully finishes when
the total size of the programing is several tens of bytes.
Thanks,
Nobuyuki
2019-02-25 10:36 AM
I would like to chime in to say I have also run into this exact same problem.
Verify did work in STM32CubeProgrammer version 1.0.0 with the exact same external flash loader (.stldr).
So something changed after 1.0.0 which causes verify to no longer work. It would be nice if this was fixed, it isn't possible to program+verify with the command line because of this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.