2019-12-03 3:19 AM
Tested chips: stm32f405rgt6, stm32f411ceu6 (DFU bootloader - internal, libusb-1.0.0).
Then I try to erase one sector or range of sectors [X Y] - it is failed:
(I remove blank lines)
"./STM32_Programmer.sh -vb 2 -c port=USB1 -e 0
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 BOOTLOADER
SN : 385C34733435
FW version : 0x011a
Device ID : 0x0413
AREA NAME SECT.NBR ADDRESS SIZE TYPE
Internal Flash 0000 0x08000000 0016 KB REW
0001 0x08004000 0016 KB REW
0002 0x08008000 0016 KB REW
0003 0x0800c000 0016 KB REW
0004 0x08010000 0064 KB REW
0005 0x08020000 0128 KB REW
0006 0x08040000 0128 KB REW
0007 0x08060000 0128 KB REW
0008 0x08080000 0128 KB REW
0009 0x080a0000 0128 KB REW
0010 0x080c0000 0128 KB REW
0011 0x080e0000 0128 KB REW
Option Bytes 0000 0x1fffc000 0016 B RW
OTP Memory 0000 0x1fff7800 0512 B RW
0001 0x1fff7a00 0016 B RW
Device Feature 0000 0xffff0000 0004 B RW
sending an abort request
setting the address pointer to address: 0x08000000
sending an abort request
setting the address pointer to address: 0x08000000
setting the address pointer to address: 0x08000000
Device name : STM32F405xx/F407xx/F415xx/F417xx
Device type : MCU
Device CPU : Cortex-M4
setting the address pointer to address: 0x08000000
Erase sector(s) ...
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
sending a clear status request
libusb control transfer error: -1
unable to switch the device to dfuIDLE/dfuDNLOAD_IDLE state
erasing sector 0000 @: 0x08000000 failed
Flash page/sector erase command correctly executed.
Note: if flash sector is protected, it will not be erased."
Then I erase all sectors - it is working good:
"./STM32_Programmer.sh -vb 2 -c port=USB1 -e all
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 BOOTLOADER
SN : 385C34733435
FW version : 0x011a
Device ID : 0x0413
AREA NAME SECT.NBR ADDRESS SIZE TYPE
Internal Flash 0000 0x08000000 0016 KB REW
0001 0x08004000 0016 KB REW
0002 0x08008000 0016 KB REW
0003 0x0800c000 0016 KB REW
0004 0x08010000 0064 KB REW
0005 0x08020000 0128 KB REW
0006 0x08040000 0128 KB REW
0007 0x08060000 0128 KB REW
0008 0x08080000 0128 KB REW
0009 0x080a0000 0128 KB REW
0010 0x080c0000 0128 KB REW
0011 0x080e0000 0128 KB REW
Option Bytes 0000 0x1fffc000 0016 B RW
OTP Memory 0000 0x1fff7800 0512 B RW
0001 0x1fff7a00 0016 B RW
Device Feature 0000 0xffff0000 0004 B RW
sending an abort request
setting the address pointer to address: 0x08000000
sending an abort request
setting the address pointer to address: 0x08000000
setting the address pointer to address: 0x08000000
Device name : STM32F405xx/F407xx/F415xx/F417xx
Device type : MCU
Device CPU : Cortex-M4
setting the address pointer to address: 0x08000000
Mass erase ...
sending an abort request
sending a full flash erase request
Mass erase command correctly executed.
Note: if there's any flash protection, it will not be erased."
dfu-util (v0.9) - working correctly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.