STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

reading flash memory

Hi, with stm32cubeprogrammer i've read flash memory, but when i want to program the micro with the file that i've read, it says that "core is locked up". what should i do to solve this problem?

Fate1 by Associate II
  • 1871 Views
  • 3 replies
  • 0 kudos

CubeIDE External Loader

Hi everyone,We're using G474 is new MCU and want to program an external flash via STM32CubeProgrammer. However, IDE can't generate valid stldr file or I have done wrong its settings. I have set the parameters as example for atollic. CubeProgrammer do...

CLI Write Protection Command

Hello,The application code is downloaded via CubeProgrammer CLI commands in my project.Now, need to protect specified pages of flash from writing.Is there a command for write protection in the current CLI of programmer? I have tried "-ob wrp=1" (for ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.