2023-10-04 12:53 PM
Hi,
I just downloaded and installed the STM32CubeProgrammer version 2.14 for linux.
The installation went without any issues. However, when I execute STM32CubeProgrammer an exception is immediately raised (see below). I tried to run it as root, but this did not help (same error).
I am connected via a terminal and an (working) X connection. The installer is used via the same terminal and connection.
I do not have any other java installation (other than the java which is installed by the STM32CubeProgrammer installer).
I have googled for this error, but I cannot find any solution for this.
Any help is much appreciated.
:/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32CubeProgrammer
Exception in thread "main" java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.launcher.LauncherHelper$FXHelper.main(LauncherHelper.java:767)
Caused by: java.lang.UnsupportedOperationException: Internal Error
at com.sun.glass.ui.gtk.GtkApplication.lambda$new$5(GtkApplication.java:158)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.glass.ui.gtk.GtkApplication.<init>(GtkApplication.java:140)
at com.sun.glass.ui.gtk.GtkPlatformFactory.createApplication(GtkPlatformFactory.java:41)
at com.sun.glass.ui.Application.run(Application.java:146)
at com.sun.javafx.tk.quantum.QuantumToolkit.startup(QuantumToolkit.java:257)
at com.sun.javafx.application.PlatformImpl.startup(PlatformImpl.java:211)
at com.sun.javafx.application.LauncherImpl.startToolkit(LauncherImpl.java:581)
at com.sun.javafx.application.LauncherImpl.launchApplicationWithArgs(LauncherImpl.java:330)
at com.sun.javafx.application.LauncherImpl.launchApplication(LauncherImpl.java:321)
... 5 more
2023-10-16 8:11 AM
Hello @daCodeMonkey ,
Thanks for your feedback,
Could you please try launching the tool with the following command:
java -jar STM32CubeProgrammer
Sara.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.