2021-02-01 1:54 AM
I'm using the STM32429I-EVAL board and STM32CubeProgammer and can program the board when the program is located in internal flash.
When I edit the app to use the external flash I get a good compile in STM32CubeIDE but the programmer will not load the bin file 'Error while reading the file'.
So I can't program the board.
ANyone had this and solved it please?
2021-02-01 2:33 AM
Not a problem I'm having.. often not a requirement
Show full error and build log to that point.
Check for spaces in path name, especially that of External Loader.
External Loader selected?
2021-02-01 2:44 AM
No compile error all ok.
Filename 'Evaluation_Example.bin' same as previously loaded and successfuiy programmed internal flash build.
M29W128GL_STM324x9I-EVAL external loader
Programmer v2.6.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.