2025-04-08 5:00 AM
If I try to write data to high-cycle flash from command line with the -w16 command when trust zone is activated it says that it succeeded but the data isn't written.
Using -w16 without trust zone works as expected.
Writing data with --download from command line works as expcted
-fillbytes works as expected from both command line and gui (though from command line I get an error saying "The data filling size must be 8, 16 or 32. 8 bit will be used by default." if I set dataWidth to 16)
Do I have to do something extra when using the -w16 command?
I'm using:
* STM32CubeProgrammer v2.19.0
* STLINK-V3SET FW V3J16M7B5S1
* STM32H56x
2025-04-17 2:55 AM
Hello @Mk4 and welcome to the Community,
Apologize for the delay.
Could you share the option bytes configuration and the command used? I'd like to make sure you are using the right address after activating the TrustZone and the eData because the area is now accessible with alias addresses.
You can refer to RM0481 section 7.3.10 "Flash high-cycle data." for further details.
Thank you in advance !
Maryem.
2025-04-17 5:15 AM
Thank you for the reply.
For trust zone i set the following option bytes:
2025-04-17 8:18 AM
Thank you for your feedback, I will further investigate from my side and get back to you shortly.
Maryem.
2025-04-22 1:23 AM
Hello @Mk4 ,
After investigating, it appears that the -w16 command is not currently supported for flash high-cycle data. As a workaround, you can use the -w or --download command instead.
A ticket has been submitted to the relevant team to address this issue. I will keep you updated on any progress.
Internal ticket number: 208220 (This is an internal tracking number and is not accessible or usable by customers)
Thank you for your understanding and patience.
Maryem.
2025-04-22 2:21 AM
Hi @Maryem
Unfortunately, using --download hits you with another bug: STM32CubeProgrammer -d erases too many sectors whe... - STMicroelectronics Community So if you are using several sectors of high-cycle count flash it is essential that you issue the download commands in strict sector order.
Best regards, Jesper
2025-04-22 8:34 AM
Hello @JesperEC ,
After reviewing, I found that this issue has already been reported. We will keep you informed of any updates.
Thank you.
Maryem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.