2019-10-05 9:17 AM
Stock hardware, and also updated with v35 ST-LINK/V3 firmware
Using MT25TL01G loader for either H750B-DISCO or H745I-DISCO External Loaders
Tried on two different machines
09:41:26 : UPLOADING ...
09:41:26 : Size : 131072 Bytes
09:41:26 : Address : 0x90000000
09:41:26 : Read progress:
09:41:31 : Error: Data read failed
09:41:51 : UPLOADING ...
09:41:51 : Size : 131072 Bytes
09:41:51 : Address : 0x90000000
09:41:51 : Read progress:
09:42:21 : Error: Data read failed
QSPI viable using my own apps, and stock demo.
Not sure the tool actually calls Init function, seen other issues where first read returns zeros, this case times out every time, never seen it read the memory.
2019-10-15 5:57 PM
Hi, sorry, doesn't looked to be fixed here, loads the code, jumps to the wrong place. GUI v2.2.0
19:45:59 : STM32CubeProgrammer API v2.2.0
...
19:46:31:506 : UPLOADING ...
19:46:31:506 : Size : 1024 Bytes
19:46:31:507 : Address : 0x90000000
19:46:31:507 : Read progress:
19:46:31:507 : Reading data...
19:46:31:548 : halt ap 0 Status = 0
19:46:31:548 : halt ap 1 Status = 32
19:46:31:555 : halt ap 2 Status = 32
19:46:31:556 : w ap 0 reg 15 PC (0x24000000)
19:46:31:556 : w ap 0 reg 17 MSP (0x24000500)
19:46:31:556 : w ap 0 reg 16 xPSR (0x01000000)
19:46:31:556 : w ap 0 @0x24001CA0 0x00000200 bytes
19:46:31:556 : w ap 0 @0x24000000 0x00000004 bytes
19:46:31:605 : w ap 0 @0x24000004 0x00001874 bytes
19:46:31:605 : Init flashloader...
19:46:31:605 : halt ap 0
19:46:31:605 : w ap 0 reg 0 R0 0x00000000
19:46:31:606 : w ap 0 reg 1 R1 0x00000000
19:46:31:606 : w ap 0 reg 2 R2 0x00000000
19:46:31:606 : w ap 0 reg 3 R3 0x00000000
19:46:31:606 : w ap 0 reg 4 R4 0x00000000
19:46:31:606 : w ap 0 reg 5 R5 0x00000000
19:46:31:606 : w ap 0 reg 6 R6 0x00000000
19:46:31:607 : w ap 0 reg 7 R7 0x00000000
19:46:31:607 : w ap 0 reg 8 R8 0x00000000
19:46:31:607 : w ap 0 reg 9 R9 0x00000000
19:46:31:607 : w ap 0 reg 10 R10 0x00000000
19:46:31:607 : w ap 0 reg 11 R11 0x00000000
19:46:31:607 : w ap 0 reg 12 R12 0x00000000
19:46:31:608 : w ap 0 reg 13 SP 0x00000000
19:46:31:608 : w ap 0 reg 14 LR 0x24000001
19:46:31:608 : w ap 0 reg 15 PC 0x2000108D
19:46:31:608 : w ap 0 reg 16 xPSR 0x01000000
19:46:31:608 : w ap 0 reg 17 MSP 0x24001C74
19:46:31:609 : w ap 0 reg 18 PSP 0x00000000
19:46:31:609 : run ap 0
19:46:36:001 : halt ap 0
19:46:36:001 : Init function fail with timeout
19:46:36:006 : r ap 0 reg 16 xPSR 0x41000003
19:46:36:109 : halt ap 0 Status = 0
19:46:36:114 : halt ap 1 Status = 32
19:46:36:114 : halt ap 2 Status = 32
19:46:36:114 : w ap 0 reg 15 PC (0x24000000)
19:46:36:114 : w ap 0 reg 17 MSP (0x24000500)
19:46:36:115 : w ap 0 reg 16 xPSR (0x01000000)
19:46:36:115 : Error: Data read failed
FromELF
========================================================================
** ELF Header Information
File Name: CLIVEONE-W25Q128B_STM32H7xx-NUCLEO-144.stldr
Machine class: ELFCLASS32 (32-bit)
Data encoding: ELFDATA2LSB (Little endian)
Header version: EV_CURRENT (Current version)
Operating System ABI: none
ABI Version: 0
File Type: ET_EXEC (Executable) (2)
Machine: EM_ARM (ARM)
Image Entry point: 0x2400108d
Flags: EF_ARM_HASENTRY + EF_ARM_ABI_FLOAT_SOFT (0x05000202)
ARM ELF revision: 5 (ABI version 2)
Conforms to Soft float procedure-call standard
Header size: 52 bytes (0x34)
Program header entry size: 32 bytes (0x20)
Section header entry size: 40 bytes (0x28)
Program header entries: 2
Section header entries: 8
Program header offset: 6836 (0x00001ab4)
Section header offset: 6900 (0x00001af4)
Section header string table index: 7
========================================================================
..
** Section #5 '.symtab' (***_SYMTAB)
Size : 112 bytes (alignment 4)
String table #6 '.strtab'
Last local symbol no. 0
Symbol table .symtab (6 symbols, 0 local)
# Symbol Name Value Bind Sec Type Vis Size
========================================================================
1 StorageInfo 0x00000000 Gb 4 Data Hi 0xc8
2 DeInit 0x24000321 Gb 1 Code Hi 0x4
3 Init 0x2400108d Gb 1 Code Hi 0x408
4 MassErase 0x24001491 Gb 1 Code Hi 0x50
5 SectorErase 0x24001775 Gb 1 Code Hi 0x80
6 Write 0x240017f5 Gb 1 Code Hi 0x18
@Houda GHABRI @Nawres GHARBI
2019-10-15 6:03 PM
Same file with CLI, does job properly
20:01:01:760 -------------------------------------------------------------------
20:01:01:761 STM32CubeProgrammer v2.2.0
20:01:01:761 -------------------------------------------------------------------
...
20:01:03:035
UPLOADING ...
20:01:03:036 File : h7_144.bin
20:01:03:037 Size : 262144 Bytes
20:01:03:039 Address: : 0x90000000
20:01:03:040 Read progress:
20:01:03:041 Reading data...
20:01:03:145 halt ap 0 Status = 0
20:01:03:146 halt ap 1 Status = 32
20:01:03:147 halt ap 2 Status = 32
20:01:03:147 w ap 0 reg 15 PC (0x24000000)
20:01:03:148 w ap 0 reg 17 MSP (0x24000500)
20:01:03:148 w ap 0 reg 16 xPSR (0x01000000)
20:01:03:152 w ap 0 @0x24001CA0 0x00000200 bytes
20:01:03:153 w ap 0 @0x24000000 0x00000004 bytes
20:01:03:194 w ap 0 @0x24000004 0x00001874 bytes
20:01:03:195 Init flashloader...
20:01:03:196 halt ap 0
20:01:03:196 w ap 0 reg 0 R0 0x00000000
20:01:03:197 w ap 0 reg 1 R1 0x00000000
20:01:03:198 w ap 0 reg 2 R2 0x00000000
20:01:03:198 w ap 0 reg 3 R3 0x00000000
20:01:03:199 w ap 0 reg 4 R4 0x00000000
20:01:03:199 w ap 0 reg 5 R5 0x00000000
20:01:03:200 w ap 0 reg 6 R6 0x00000000
20:01:03:200 w ap 0 reg 7 R7 0x00000000
20:01:03:201 w ap 0 reg 8 R8 0x00000000
20:01:03:201 w ap 0 reg 9 R9 0x00000000
20:01:03:202 w ap 0 reg 10 R10 0x00000000
20:01:03:202 w ap 0 reg 11 R11 0x00000000
20:01:03:203 w ap 0 reg 12 R12 0x00000000
20:01:03:203 w ap 0 reg 13 SP 0x00000000
20:01:03:204 w ap 0 reg 14 LR 0x24000001
20:01:03:204 w ap 0 reg 15 PC 0x2400108D
20:01:03:205 w ap 0 reg 16 xPSR 0x01000000
20:01:03:205 w ap 0 reg 17 MSP 0x24001C74
20:01:03:206 w ap 0 reg 18 PSP 0x00000000
20:01:03:206 run ap 0
20:01:03:207 halt ap 0
20:01:03:208 r ap 0 reg 0 R0 0x00000001
20:01:05:027 r ap 0 @0x90000000 0x00040000 bytes
20:01:05:028
Data read successfully
20:01:05:031 Time elapsed during read operation is: 00:00:01.988
2019-10-15 6:44 PM
Trying to do a full read of the device stops after the first complete RAM buffer fill of 0x7E000
https://community.st.com/s/question/0D50X0000BTf3v0SQB/stm32-cube-programmer-v220-still-buggy
@Houda GHABRI
2019-10-16 2:20 AM
Hi Clive,
can you provide me command line you are using?
Best regards,
Houda
2019-10-16 3:08 AM
The command line input is shown approximately in the other thread, the path for the external loader was truncated for clarity.
The first test I had read 0x40000 bytes, after that looked to work I pushed it to 0x1000000. The file was 16MB in size, but only the first 0x7E000 bytes were valid.
I will note the equivalent command line on the old ST-LINK Utilities does successfully read the whole 16MB device.
2019-10-16 3:59 AM
Hi Clive ,
As answered in this thread https://community.st.com/s/question/0D50X0000BTf3v0SQB/stm32-cube-programmer-v220-still-buggy
i confirm there is issue to read big data .
The Cubeprogrammer development team is aware of this problem and will be corrected shortly.
Feel free to contact me for furthers details.
Regards,
houda
2020-08-30 4:10 PM
This continues to be a problem.
The first time it loads the .ELF it gets the Init address wrong, the second time (after disconnect/connect) it loads correctly.
This seems specific to the H7 where the STLDR are put in the 0x24000000 RAM rather than 0x20000000
2020-09-08 7:44 PM
@Houda GHABRI
2020-12-02 8:21 AM
@STOne-32 UP
https://community.st.com/s/question/0D53W00000OpGGsSAN/stm32h743-external-loader-problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.