2023-08-10 6:37 AM
System: Macbook Pro M2 OS Ventura 13.4.1 and ST-Link Server 2.1.
I can't access the serial port of the STLink nor with the ST32Programmer because it doesn't recognize the STLink correctly. On my Intel Mac with OS Ventura there are no problems.
Does anyone know a solution , thanks in advance
2023-08-10 6:51 AM
I've forgotten to attach the output of the Programmers log:
15:46:14 : STM32CubeProgrammer API v2.13.1 | MacOS-64Bits
15:46:24 : UR connection mode is defined with the HWrst reset mode
15:46:24 : ST-LINK SN : 004500213431511037393330
15:46:24 : ST-LINK FW : V3J12M3
15:46:24 : Board : DISCO-H747XI
15:46:24 : Voltage : 3.25V
15:46:24 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
2024-02-11 11:51 PM
I have the same problem. It's been 6 months and ST hasn't responded to your question, which is appalling. My $2 Chinese STLink clone works with STM32CubeProgrammer, but the original STLink V3 MiniE doesn't. Moreover, when I updated the Chinese STLink through STM32CubeProgrammer, it also stopped working with my M2 MacBook. I conclude that ST does not support this platform but sells STLink without warning customers. If you have an ARM MacBook, you are buying a device that will not work.
2025-01-28 6:41 AM
Hi @devellevel
Did you ever solve this issue? If not, check this FAQ, it might be helpful!
FAQ: Possible communication failure between STLINK... - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.