2025-12-09 9:22 PM
Hello
I am connecting the ST-LINK and downloading the firmware to the programmer.
I have a question. Can I do power from ST-LINK and download firmware instead of supplying external power to the MCU? Currently, I use external power, but I wonder if there is such a way.
Thank you.
Solved! Go to Solution.
2025-12-09 10:39 PM - edited 2025-12-09 10:41 PM
Hi,
A genuine st-link has no power output, so no power for the target.
Only if you solder/wire a connection to get power yourself, let say with a st-link V3 mods, you can have some 100mA or so from the st-link. See the manual for st-link V3mods.
2025-12-09 10:39 PM - edited 2025-12-09 10:41 PM
Hi,
A genuine st-link has no power output, so no power for the target.
Only if you solder/wire a connection to get power yourself, let say with a st-link V3 mods, you can have some 100mA or so from the st-link. See the manual for st-link V3mods.
2025-12-10 1:17 AM
You didn't say what ST-Link you're using - there are several versions:
TN1235: Overview of ST-LINK derivatives
Those are the real ones; there are also fakes/clones - see: How to recognize a genuine ST-LINK/V2 versus a cloned one.
The User Manual for the particular model you have will describe its capabilities...
2026-01-13 7:26 AM - edited 2026-01-13 7:26 AM
Hi @giwonKIM,
Along with comments said by @Andrew Neil and @AScha.3, there's also the STLINK-V3PWR that can power the STM32.
If any of these answers address your question, please mark the comment as accepted solution.
Thanks in advance,
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.