2026-01-20 8:24 AM
Hi everyone,
I'm working on a power conversion project using the STEVAL-7BIDIRCB reference design.
The firmware uses a specific static library: DPC_AverageCurrentCtrl_IAR.a. As the name suggests, it was compiled with IAR EWARM. However, I would like to use VS Code and CMake for my development environment instead of the IAR IDE.
A few questions:
Is this specific library compatible with the arm-none-eabi-gcc linker in a CMake setup, or will I face ABI/runtime issues (especially regarding FPU and math functions)?
If I use the IAR Build Tools (compiler/linker) through CMake in VS Code, will it work seamlessly with this .a file?
Is there a GCC version of this library available for the STEVAL-7BIDIRCB, or are the sources available somewhere to recompile it for GCC?
The control loop is obviously critical for this board, so I want to make sure I don't introduce any instability by mixing toolchains.
Thanks for your help!
2026-02-11 5:26 AM
hi @simon_12542
you should treat it as incompatible as:
IAR and GCC use different ABIs:
Different name mangling rules (for C++, if any).
Different conventions for:
Function prolog/epilog
Passing/returning structs, 64‑bit types, floating‑point values
Use of registers vs. stack, especially with FPU.
Runtime dependencies differ:
An IAR static library usually depends on IAR’s C runtime (DLib / CLib), their math implementations, and startup assumptions.
GCC code expects newlib or newlib-nano, different libm, different startup.
Even if the .a is “just” ARM code, the object files inside are built against IAR’s ABI and runtime. Mixed-toolchain linking is not supported
what we recommend as approach:
arm-none-eabi-gcc):
DPC_AverageCurrentCtrl_IAR.a.DPC_AverageCurrentCtrl_IAR.a). That’s precisely the kind of subtle problem that can manifest as unstable current/voltage control under load transients.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.