2024-07-04 12:57 AM - last edited on 2024-07-08 4:51 AM by Peter BENSCH
Hello ST community
I'm trying to install SetupSTM32CubeProgrammer-2.16.0.linux in docker
But getting error like below
root@1694a12cc06d:/home/app/en.stm32cubeprg-lin-v2-16-0# ./SetupSTM32CubeProgrammer-2.16.0.linux
./SetupSTM32CubeProgrammer-2.16.0.linux
/home/app/en.stm32cubeprg-lin-v2-16-0
chdir /home/app/en.stm32cubeprg-lin-v2-16-0/.
current dir /home/app/en.stm32cubeprg-lin-v2-16-0
SEVERE: com.izforge.izpack.api.exception.IzPackException: Console implementation not found for panel: com.st.CustomPanels.AnalyticsPanels
Thanks in advance.
Solved! Go to Solution.
2024-11-28 5:20 AM
Hello @parshv22,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.
2024-08-20 1:56 AM
Hello @parshv22,
I apologize for the delayed response.
This error generally occurs when trying to install CubeProgrammer in an environment that lacks a user graphical interface. Unfortunately, it's not possible to install the tool without using the GUI installer or in silent mode at this time. A request has already been submitted to our development team to support this feature. I will keep you updated on any progress.
Maryem.
2024-08-20 2:18 AM
Dear Maryem,
Thank you for your response and for clarifying the situation regarding the installation of CubeProgrammer.
I understand that the tool requires a graphical user interface for installation and that the current version does not support silent mode. I appreciate your efforts in requesting this feature from the development team and would be grateful if you could keep me informed about any updates or potential solutions.
If there are any interim steps or alternative methods you could suggest for environments without a GUI, I would be very interested in exploring those options.
Thank you once again for your assistance.
Thanks & Regards
Parshv Ajmera
2024-11-28 5:20 AM
Hello @parshv22,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.
2024-12-05 4:37 AM
Hello @Maryem
I apologize for the delayed response.
Thanks for the update.
Thanks & Regards
Parshv Ajmera
2025-09-08 12:28 AM
Hello @Maryem,
what will be the install command for starting the SetupSTM32CubeProgrammer-2.20.0.linux to install it in cli mode? I am not able to find some documentation to this issue.
2025-11-25 1:12 AM
Same here, I do not figure out how to install the programmer in silent mode on linux station (docker environment).
Regards
2025-11-25 7:30 AM
Hello @CTare.1 @janfrischling9 ,
To install STM32CubeProgrammer from the command line, please refer to Section 1.2.7 of the User Manual, where detailed steps are provided.
Feel free to reach out if you encounter any issues.
Thanks,
Amine.
2025-11-25 7:32 AM
2025-12-03 1:32 AM
@Amine_Jridi Could you explain how, under linux, docker it should work as of v2.18?
I am currently using the v2.21 zip file for linux (Part of the Dockerfile, note that I have all dependencies for stm32programmer installed as well)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.