2026-02-03 10:36 PM
I am working on an STM32H563 project with a custom bootloader and two application slots (APP1 / APP2).
This is my memory layout
The bootloader is already deployed in the field and cannot be modified.
The bootloader jump sequence is standard:
This works perfectly when I build the application the “manual” way:
I would like to automate this process using cmake , without manually editing the linker script and system_stm32h5xx.c
So I implemented:
target_compile_definitions(app1 PRIVATE
VECT_TAB_OFFSET=0x00022000
)In the linker template .ld.in file, i have this:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
FLASH (rx) : ORIGIN = @FLASH_ORIGIN@, LENGTH = @FLASH_LENGTH@
}FLASH_ORIGN and FLASH_LENGTH are the variables
The generated .ld correctly shows FLASH (rx) : ORIGIN = 0x08022000, and i checked using STM32 cube programmer that the hex file is programmed at the correct address.
The problem is that when i generate the hex files from cmake , once i flash them in , the bootloader does not jump to the application.
Am i missing any obvious step here? I have attached the cmakelist file and the linker template(STM32H563xx_FLASH.ld.in)
Kindly Help
Solved! Go to Solution.
2026-02-04 3:03 AM
The common reason for that kind of failure is the unreasonable setting of VTOR in SystemInit() routine.
The easiest fix is to put the statement at the very start of main():
extern struct cm_vectable_ g_pfnVectors;
SCB->VTOR = (uint32_t)&g_pfnVectors;
2026-02-04 3:03 AM
The common reason for that kind of failure is the unreasonable setting of VTOR in SystemInit() routine.
The easiest fix is to put the statement at the very start of main():
extern struct cm_vectable_ g_pfnVectors;
SCB->VTOR = (uint32_t)&g_pfnVectors;
2026-02-04 10:12 PM
Thanks , Once i manually set the SCB->VTOR in main , i am now able to jump properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.