2025-06-29 2:40 AM - edited 2025-07-17 11:54 PM
Hi,
I'm trying to work with the STM32N6. I have a NUCLEO-N657X0-Q board.
When I use an external debugger via CN1 everything is fine, however I am experiencing a lot of trouble with the ST-Link.
It seems like there is a small (0.01%) chance that attempting to access memory will cause the device to lock up.
An example of the sort of command that gets sent to the ST-Link is: `[0xf2, 0x07, 0xfc, 0xff, 0x00, 0x34, 0xcc, 0x35, 0x01]`. That is, a simple command to the ST-Link to read or write memory.
I am doing this as part of an attempt to implement support for the STM32N6 for probe-rs, however the problem seems to occur even when using ST tools. For example, the following has a good chance of locking up:
./STM32_Programmer_CLI \
-c port=swd \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768 \
-r32 0x34000000 32768Once the ST-Link has locked up, the only way to get it back is to unplug it and plug it in again. Any attempt to access the ST-Link USB endpoint will be met with silence.
In the example I've attempted to read main memory, however I see similar lockups when attempting to read ROM, or even when attempting to read register values repeatedly such as (to pick a random peripheral) 0x56028048, or even trying to read something from the ARM CoreSight block such as 0xE000ED14.
I am running ST-Link firmware V3J16M8 on the integrated debugger. This seems like it's a bug in the ST-Link, because running the link at a lower frequency reduces the failures. For example, they seem to go away entirely at around 100 kHz.
This issue only occurs when the device is attached directly to a USB-C port on the Mac. It goes away on other platforms, and it goes away when it is behind a hub.
Solved! Go to Solution.
2025-12-14 9:38 AM
Dear @sean_od ,
The behavior observed is linked to the Errata described in this Knowledge Article FAQ : FAQ: Possible communication failure between STLINK... - STMicroelectronics Community
Let us know
STOne-32.
2025-07-17 11:53 PM
The same command appears to work when run from a Linux host. Additionally, it works from the Mac if I put a USB-C hub in between.
The problem then becomes: The ST-Link locks up when connected directly to a USB-C port on a Mac.
Are there any known issues regarding this?
2025-12-14 9:38 AM
Dear @sean_od ,
The behavior observed is linked to the Errata described in this Knowledge Article FAQ : FAQ: Possible communication failure between STLINK... - STMicroelectronics Community
Let us know
STOne-32.
2025-12-14 5:25 PM
Thanks for the link! This does seem to be the case. I'll add a check to alert if we're trying to use a device when connected directly to the machine, and advise the user to use a hub.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.