2025-06-23 1:14 AM
When I try to install the CubeProgrammer, I get the following error message:
“SetupSTM32CubeProgrammer-2.19.0” is damaged and can’t be opened. You should move it to the Trash.
I get the same error message when I unzip and double click in the finder or use the terminal with zsh or bash. I also tried version 2-18 and 2-17 with the same result.
I have successfully install CubeIDE and CubeMX.
2025-07-07 3:22 AM - edited 2025-07-07 5:10 AM
Hello @Nystrom.Eric
STM32CubeProgrammer v2.20 is out and there's a specific new package for macOS on ARM processors. Could you try it out and let us know if the issue is resolved?
Here's the link STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics.
Thanks,
Aziz
2025-07-26 10:44 AM
I think the problem might not be solved with 2.20.0
I had this problem because my file system is case sensitive.
How come ST cannot deliver a macOS app working on case sensitive file system when having the application available for linux ???????????
My solution was to install it on an external disk with case insensitive file system than making a disk image that I can access from my internal disk.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.