2024-07-09 4:30 AM
Hi,
When installing STM32CubeProgrammer on a Linux machine with a graphical interface, an installation window appears. Now, I want to install STM32CubeProgrammer on a Linux machine without a graphical interface. When I run the installer, I get this error message:
Command line arguments:
SEVERE: com.izforge.izpack.api.exception.IzPackException: Console implementation not found for panel: com.st.CustomPanels.AnalyticsPanels
How can I install STM32CubeProgrammer without the need for a graphical interface?
Best regards,
Solved! Go to Solution.
2024-11-28 5:17 AM
Hello @mikel-m,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.
2024-07-09 7:12 AM
Hello @mikel-m,
It is currently not possible to install CubeProgrammer without using the GUI installer or in silent mode. A request has already been submitted to our development team to support this feature. I will keep you updated on any progress.
Internal ticket number: 186141 (This is an internal tracking number and is not accessible or usable by customers).
Maryem.
2024-11-28 5:17 AM
Hello @mikel-m,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.