2018-09-14 3:18 AM
The following defines an Intel hex file that should program Internal memory at 0x08018040 with:
0xFFFFFFFF, 0x00001520, 0xFFFFFFFF, 0xFFFFFFFF
:020000040801F1
:10804000FFFFFFFF20150000FFFFFFFFFFFFFFFF07
:00000001FF
When I use the Cube programmer to load this into the processor I find that the memory at 0x08018050 is set to:
0x00DB385E, 0x00000000, 0x73617265, 0x30203A65 in addition to the desired operation
2018-10-08 6:52 AM
Hello,
Is it possible for you to share the hex file you used for test?==
Compared to STLink Utility, do you confirm that there is no such issue?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-10-26 1:06 AM
The three lines above are valid Intel Hex and are the contents of the problem file. With the ST-Link utility there does not seem to be a problem.
2018-10-26 4:23 AM
Which IDE do you use?
2018-10-26 7:58 AM
This hex data is generated from a binary image that defines some constants that have to be set at a fixed location in memory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.