2020-08-17 8:36 PM
I've been trying to use TIM1CH2N to generate PWM to control ws2812b RGB LED. I have got one working library for TIM1CH2, but I'm unable to generate the same signals in the CH2N pin (STM32H750VB). Can anyone help me out to resolve this issue?
Solved! Go to Solution.
2020-08-18 9:31 PM
Issue was with my function, earlier I used HAL_TIM_PWM_Start(); function to start pwm, the actual one i should use is HAL_TIMEx_PWMN_Start(); to generate pwm signal on complementary configuration.
2020-08-17 9:45 PM
To get both complementary outputs working, all you need is to set TIM1->CCER.CC2NE and set up the respectve pin in GPIO.
JW
2020-08-18 9:31 PM
Issue was with my function, earlier I used HAL_TIM_PWM_Start(); function to start pwm, the actual one i should use is HAL_TIMEx_PWMN_Start(); to generate pwm signal on complementary configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.