2022-06-07 2:43 AM
Hi all,
I realized my custom external loader for STM32CubeProgrammer and it works fine when used from the Programmer GUI.
I can program, erase ad read external flash.
Now I'd like to use the command line interface but I cannot find how to mass erase the external flash from CLI.
If I load a .HEX file for the external flash the affected sectors are erased and programmed perfectly, but issuing the -e all command anly erases the internal flash.
Since my .hex file contains only used external flash areas, I'd like to do a mass erase before writing so I'm sure that flash is clean before writing.
External mass erase is possible from GUI so I suppose it is also possibel from command line...
Any suggestion?
Thanks,
Davide
Solved! Go to Solution.
2022-06-30 9:15 AM
Hello @Community member,
Thank you for posting,
You can achieve this by using the following command :
STM32_Programmer_CLI.exe -c port=swd -e all -el "Absolute path of your external loader"
Keep in mind that this command is only available when using SWD/JTAG.
I hope this helps.
Best regards,
Aziz
2022-06-30 9:15 AM
Hello @Community member,
Thank you for posting,
You can achieve this by using the following command :
STM32_Programmer_CLI.exe -c port=swd -e all -el "Absolute path of your external loader"
Keep in mind that this command is only available when using SWD/JTAG.
I hope this helps.
Best regards,
Aziz
2024-04-24 2:33 AM
How does erase all behave when i am passing my external loader binary?
Will it only erase the external flash, or also cause an erase of the internal flash?
Do i have to call an erase for external and internal flash separately?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.