2021-09-20 8:13 AM
I'm using this command for Tx, and please let me know if I'm using correct clock config as well.
uint8_t csend[] = {0x00,0x00,0x27,0x10}; // Tx Buffer
HAL_CAN_AddTxMessage(&hcan,&txHeader,csend,&canMailbox); // Send Message
Clock config:
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI14|RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.HSI14State = RCC_HSI14_ON;
RCC_OscInitStruct.HSI14CalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI48;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
I also get this in debugger console
Debugger connection lost.
Shutting down...
2021-09-21 2:45 AM
Hello @SPati.9 ,
I think your issue is related to STM32CubeProgrammer issue.
I advise you to check these posts: post1 and post2.
Hope this helps!
Please keep me informed about your update on this issue.
Imen
2021-09-21 7:54 AM
It did not work, still
Debugger connection lost.
Shutting down...
I've tried resetting from STM32 programmer, mass_erase, software system reset in debugger and reinstalling Cube IDE as well. I'm using MAC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.