2022-01-17 7:46 PM
I have STM32H753XI-EVAL2 board with CN2(USART1) connected to PC. Switch 1 position is set to 1(Sys Mem).
I am getting error when tried to connect using STM32 CubeProgrammer.
19:43:22 : RTS low
19:43:22 : DTR low
19:43:22 : Serial Port COM18 is successfully opened.
19:43:22 : Port configuration: parity = even, baudrate = 9600, data-bit = 8, stop-bit = 1.0, flow-control = off
19:43:24 : Timeout error occured while waiting for acknowledgement.
19:43:24 : Timeout error occured while waiting for acknowledgement.
19:43:24 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
Did anyone observe the same?
2022-01-20 10:28 AM
Note that USART1 on this board has dual connection: it can be routed to the DB9 serial connector or to ST-LINK as a "virtual COM port".
This is selected by two jumpers. Make sure that the jumpers are installed as you need.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.