2023-07-28 3:09 AM - edited 2023-07-28 4:27 AM
I am working with a NUCLEO-WB15CC, and it seems that I can't read or write anymore. When I connect via ST-Link in STM32CubeProgrammer (v2.14.0) I just get
Error: Data read failed
When I try to read registers, I get the same error.
I also can't erase the chip:
Error: Mass erase operation failed.Please verify flash protection
RDP option byte is AA, so that can't be the problem.
For write protection, I don't really remember what the default values was, but they are: 0xff, 0x0, 0xff, 0x0,
I can still see target information in Programmer but nothing else seems to work, have I bricked the chip?
Edit: I noticed I also can't read registers via the CLI, so maybe it's not a bug in STM32CubeProgrammer.
This is the command I used:
STM32_Programmer_CLI.exe" -c port=SWD -r32 0x08000000 0x4
Which results in
Error: failed to read the requested memory content
Read protection seems to be disabled:
Here are all the option bytes:
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
User Configuration:
nBOOT0 : 0x1 (nBOOT0=1)
nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
SRAM2RST : 0x1 (SRAM2 is not erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWDGSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
GPIO_MODE_PB11: 0x1 (If RESET_MODE_PB11 = 0: Standard GPIO pad functionality, Only internal RESET possible. If RESET_MODE_PB11 = 1: Bidirectional reset, NRST pin configured in reset input/output mode (default mode), GPIO functionality is not available on PB11.)
RESET_MODE_PB11: 0x1 (If GPIO_MODE_PB11 = 0: Reset input only, a low level on the NRST pin generates system reset, internal RESET not propagated to the NSRT pin. If GPIO_MODE_PB11 = 1: Bidirectional reset, NRST pin configured in reset input/output mode (default mode).)
IRH : 0x1 (Internal resets drives NRST pin low until it is seen as low level.)
ESE:
ESE : 0x1 (Security enabled)
PCROP Protection:
PCROP1A_STRT : 0x1FF (0x807FC00)
PCROP1A_END : 0x0 (0x8000400)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
PCROP1B_STRT : 0x1FF (0x807FC00)
PCROP1B_END : 0x0 (0x8000400)
Write Protection:
WRP1A_STRT : 0x18 (0x800C000)
WRP1A_END : 0x20 (0x8010000)
WRP1B_STRT : 0xFF (0x807F800)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1
IPCCDBA-AA:
IPCCDBA : 0x3FFF (0x20013FFF)
OPTION BYTES BANK: 2
Security Configuration Option bytes:
SFSA : 0x0 (0x8000000)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
BRSD_B : 0x0 (SRAM2b is secure)
SBRSA_B : 0x0 (0x20038000)
BRSD_A : 0x0 (SRAM2a is secure)
SBRSA_A : 0x0 (0x20030000)
SBRV : 0x13E00 (0x8000000)
Solved! Go to Solution.
2023-07-31 11:22 PM
I "fixed" this by running this command to reset the board to factory settings:
STM32_Programmer_CLI.exe -c port=SWD reset=HWrst -w32 0x5800040c 0x00008000
2023-07-31 11:22 PM
I "fixed" this by running this command to reset the board to factory settings:
STM32_Programmer_CLI.exe -c port=SWD reset=HWrst -w32 0x5800040c 0x00008000
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.