2025-03-17 12:20 PM
Hello,
after changing one of the BCM4/7 boot option bytes of my Nucleo STM32H755 board with STM32CubeProgrammer, I can't connect to the MCU any more. When trying to connect with STM32CubeProgrammer, I get
Error: Unable to read device id from ROM table
Error: ST-LINK error (DEV_CONNECT_ERR)
Is this related to the change in option bytes or did the board get damaged somehow?
Thanks and regards,
Martin
Solved! Go to Solution.
2025-03-17 1:24 PM
Try connecting using access port 3 instead of access port 0.
2025-03-17 1:24 PM
Try connecting using access port 3 instead of access port 0.
2025-03-18 12:25 AM
Wow, this works, thanks a lot!
I just double checked: When I turn option BCM7 back on I can connect again on port 0. When I turn BCM7 off I can only connect on port 3.
2025-03-18 1:39 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.