STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Bug with latest version and STM32G0B1KB MCU

When attempting to program an STM32G0B1KB MCU (128kB of flash) with the latest version of STM32CubeProgrammer (2.13.0) the target information flash size says it only has 63kB of flash. This is not a valid flash size for this family of MCUs, and it do...

_legacyfs_online_stmicro_images_0693W00000bkSQWQA2.png _legacyfs_online_stmicro_images_0693W00000bkSQgQAM.png
RHelv.1 by Associate III
  • 1685 Views
  • 1 replies
  • 0 kudos

How to Enter boot loader in STM32H743BIT6 via USART1? pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V). the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

How to Enter boot loader in STM32H743BIT6 via USART1?pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V).the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

ZSade.1 by Associate II
  • 4709 Views
  • 6 replies
  • 0 kudos

Resolved! Error: Problem occured while trying to connect

l want to connect pcb board through stm32cubeprogrammer.But it posts pop-up like that.The error massage is "Error: Problem occured while trying to connect".And sometimes it connects well, so i can't find the reason.Could you give me some adivce to th...

_legacyfs_online_stmicro_images_0693W00000bjotnQAA.png
jju.1 by Associate II
  • 7625 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.