STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Flash Memory program

Dear @KDJEM.1 when I read the manual "rm0432" It is given thatThe Flash memory programming sequence in standard mode is as follows:1. Check that no Flash main memory operation is ongoing by checking the BSY bit in theFlash status register (FLASH_SR)....

flash.png
ajimathew by Associate III
  • 2371 Views
  • 1 replies
  • 1 kudos

Resolved! HAL interrupt function

Dear @KDJEM.1 Whenever, I implement the HAL_Interrupt functions(say HAL_UART_Receive_IT();). What is happening at the backend, to use those interrupt function I should enable the global interrupt (NVIC) in CubeIDE. What are these global interruptsals...

ajimathew by Associate III
  • 6633 Views
  • 5 replies
  • 6 kudos

Loading WAV file with CubeProgrammer

I need to load a few small audiofiles to the flash memory of STM32F407VGT6 on my F4Discovery board and now I am curious about one thing. Is it possible to load WAV samples with STM32CubeProgrammer?For example, if I use xxd command in Ubuntu to conver...

bug in stm32cubeProgrammer version v2.13.1

Hi, I found a bug in stm32cubeProgrammer version v2.13.1. When you try to readout unprotect an STM32H7A (without smps) and if its rdp level is set to 1, that didn't works. I have to unlock it manually inside my software.  

Nnabb.1 by Associate II
  • 993 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.