STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32L431 CANBUS Bootloader with stlinkv3-pwr

I attempted to flash my STM32L431 using an ST-Link v3 with STM32CubeProgrammer. I've connected the CRX pin to PB8 and the CTX to PB9, with BOOT0 set high. Despite successful attempts using SPI and USART, flashing via CAN always results in errors. I'v...

bill029 by Associate
  • 1333 Views
  • 1 replies
  • 0 kudos

Installing SFI remotely on NUCLEO-U575ZI-Q

Hi,I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does...

mikel-m by Associate III
  • 1096 Views
  • 1 replies
  • 0 kudos

Resolved! Which Device can I use for debugging STM32F105VCT6

Hi All,I am new for STM32F105VCT6. When I want to debug by using STM32CubeProgrammer, I can not see devices list for STM32F105 as picture.My question is can I select STM32F107 for debug STM32F105. If it can not, What should I use for dubugging STM32F...

Screenshot 2024-09-28 102907.png
WPong.1 by Associate III
  • 1132 Views
  • 1 replies
  • 2 kudos

SetupSTM32CubeProgrammer-2.17.0.exe failed

I got this error message when trying to install the cube programmer:This application was configured to use a bundled java runtime environment but the runtime is missing or corrruptedI have started an jar file to see if my local jre is broken which is...

HeinzH_0-1720015336386.png HeinzH_1-1720015437731.png
HeinzH by Associate
  • 3367 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.