cancel
Showing results for 
Search instead for 
Did you mean: 

Installing SFI remotely on NUCLEO-U575ZI-Q

mikel-m
Associate III

Hi,

I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.

Best regards and thanks in advance.

1 REPLY 1
ollipop
Associate II

@mikel-mehall wrote:

Hi,

I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.

Best regards and thanks in advance.


To install the SFI file remotely on your NUCLEO-U575ZI-Q, you typically need a method to flash the firmware without being directly connected to a PC running STM32CubeProgrammer. While STM32CubeProgrammer is primarily designed for local installations. Hope! it would be helpful.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.